This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LOG manager implicit instrumentation APIs



How can I obtain the LOG manager implicit instrumentation APIs ?

and find out the LOG object / buffer internal data structure  ?

I am trying to implement a Linux software tool that can read the user defined LOG buffer in the DSP/BIOS, and display the log messages on the Linux console.

As shown in Figure 3-2 in the "SPRU423F" DSP/BIOS User's Guide, section 3.3.2 page 3-8:

" ... LOG buffers are read from the target and stored in a much larger buffer on the host. Records are marked empty as they are copied up to the host. "

I think the CCS plug-in (DSP/BIOS --> Message Log) running on windows is interfacing with the LOG manager implicit instrumentation APIs for retrieving the log messages from the log buffer. I would like to implement the same feature (limited to only user-defined logs)   but on Linux platform.  

Thanks,

/Chi.