This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100v2 "Blackhawk" same as TMDSEMU100V2U-20T?

Hello,

I am trying to figure out which JTAG emulator to purchase.  I have a Beaglebone Black rev. B (Cortex A8) and I will be using it to develop some ARM assembly this summer using CCS 5.5.  I understand that I need to order the SAMTEC FTR-110-03-GD-06 and then I also need to get the JTAG emulator.  Is TMDSEMU100V2U-20T the emulator that I need?  It appears to be the correct one, but I can't seem to find an image that will enlarge for verification.  I was also told that I should get the "Blackhawk" one.  Is this one the "Blackhawk" model?  Or should I be ordering http://store.blackhawk-dsp.com/default/usb100v2d-jtag-emulator.html#!prettyPhoto straight from Blackhawk?  Any help is appreciated.

Thanks,
Jeff