Ported the android JB 4.1.2 , the board is up. Installed some opencv application (USB Camera capture application). But the IPU is crashing when the opencv application is launched. What could be the reason not able to understand ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ported the android JB 4.1.2 , the board is up. Installed some opencv application (USB Camera capture application). But the IPU is crashing when the opencv application is launched. What could be the reason not able to understand ?
Hi
Can you please paste the crash log instead of a screenshot?
Regards,
Boyko
ok.. here is my attached log. 8562.log.txt can someone help me out . Moreover the IPU is crashing when any application related to camera is running the inbuilt Cameraomap app, which is available from source code itself.
Regards,
Sainath
Hi Sainath,
what ducati version are you using?
More on how to update it see here:
http://www.omappedia.com/wiki/4AJ.2.2_OMAP4_Jelly_Bean_Panda_Notes#Updating_Ducati
http://omappedia.org/wiki/Ducati_For_Dummies
Hi ,
To make the opencv camera application work, do I need to add Ducati. After applying this binary does IPU won't crash ..? If so, actually I'm using the variscite DART Board.
Regards,
N Sainath
Hi
Thanks for your support I have applied the ducati binary. Know the IPU is not crashing but the opencv application says that " your device doesnot have camera support (or) it is locked " & the log is says " failed to disable tw16040 MCLK "
Regards
N Sainath
Hi Boyko,
kernel version 3.0.31 ,
opencv CV 2.4.9
android JB 4.1.2
Regards,
sainath
Hi
can you please check out my log & help me why my camera application is crashing on 4460 based board. here is my log. 4812.Log_v.txt
Regards,
Sainath