This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x MPlayer compile error

Hello,

We are using the Linux SDK 07.00.00.00 and we like to compile mplayer to use on our board.

I followed this guide: http://processors.wiki.ti.com/index.php/Mplayer and give the following configur command:

./configure  --enable-cross-compile --cc=arm-linux-gnueabihf-gcc --host-cc=gcc --as=arm-linux-gnueabihf-as --ar=arm-linux-gnueabihf-ar --ranlib=arm-linux-gnueabihf-ranlib --target=arm-linux --enable-alsa

The path to the arm-linux-gnueabihf- is exported so could be acces and I use Ubuntu 12.04.

When I make I get an Z_NO_COMPRESSION error in the vo_png.c, so I configured again with the --disable-png added to it.

Then I run make again and I get an error in vo_ivtv.c in function 'ivtv_reset', 'sd' and 'sd1' isn't known, IVTV_STOP_FL_HIDE_FRAME error and few in vo_ivtv.c

What can I do to compile this correctly

Thanks in advance

Patrick