Are these bits in DDR3 Memory Controller Status Register sticky?
RDLVGATETO
RDLVLTO
WRLVLTO
IFRDY
Assuming I used Full Leveling with incremental leveling turned on, say the read data leveling timeout initially and RDLVLTO is set to zero, does it get set to 1 if the subsequent incremental level converges the read data eye training? Say my DDR3 PHY is initially lock but somehow loses lock and required lock again, does IFRDY bit goes from 1 to 0 and back to 1?
Thanks,
Chris