This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omap4 + camera

Hi ,

I have compiled the android JB 4.1.2 source code. The blaze(omap4460) is up . All the inbuilt applications included in the source are working fne. But the only problem with the camera application, on invoking the camera application the application is crashing. Added the ducati binary also. On bootup in the debug messages there are some IPU error. Is that something to be worried or not. I'm using the USB camera & its being detected by kernel as /dev/video but no capture of image OR preview by usb camera. 

Also on running the opencv camera capture application the application says "  device doesnot have camera support or it s locked " . I want to make this opencv application work. can any one help me out to overcome this problem.7701.camera.txt

My log...

7041.camera.txt