This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Am335x EVM with ramfs

Hi,

I am trying to boot AM335x EVM with ramfs support but its showing error as,

[    2.340570] VFS: Mounted root (ramfs filesystem) on device 0:13.
[    2.347131] devtmpfs: error mounting -2
[    2.351770] Freeing unused kernel memory: 332K (c0778000 - c07cb000)
[    2.358542] Failed to execute /sbin/init.  Attempting defaults...
[    2.365030] Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

i have copied the ramfs to 0x80100000


my u-boot arguments are,

Kernel command line: console=ttyO0,115200n8 root=/dev/ram0 rw initrd=0x80100000,58M rootfstype=ramfs init=/sbin/init

can any one please tell me whrere i am going wrong.