Hi,
I would like to confirm whether C672x ROM BIOS is supported on DA7xx or not.
I tried it by following the recipe described in http://www.ti.com/lit/an/spraas8/spraas8.pdf,
but I could not run my application successfully. Please note my application is working with RAM based BIOS on DA7xx EVM.
My understanding is that DA7xx and C672x is almost same in HW point of view.
I know some differences should be present in ROM image, for example, DA7xx has some additional libs in ROM.
I wondered that the address mapping of ROM image would be same between these devices, but it seems my assumption is incorrect considering the result of my trial...
Best Regards,
Kawada