Hi.
I am using SYS / BIOS and TMDSSK3358.
I attach the project.
Data Abort occurs when you run the line 16 "led.c".
log:
[CortxA8] Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x80010204.
Main stack size: 0x1000.
R0 = 0x0000005f R8 = 0x000a0000
R1 = 0x44e10854 R9 = 0x00000000
R2 = 0x800037dc R10 = 0x000298d0
R3 = 0x00000000 R11 = 0x000298d0
R4 = 0x4030cfd8 R12 = 0x0000005f
R5 = 0x0001dc4f SP(R13) = 0x800111f0
R6 = 0x48040000 LR(R14) = 0x80008124
R7 = 0x4030fca0 PC(R15) = 0x80001a7c
PSR = 0x6000019f
ti.sysbios.family.arm.exc.Exception: line 176: E_dataAbort: pc = 0x80001a7c, lr = 0x80008124.
xdc.runtime.Error.raise: terminating execution
Is it possible to abort data so as not to cause How do I?
Best Regards,
hamada