Other Parts Discussed in Thread: AM3358, TPS65910, DA8XX
Hi,
I am trying to boot by SD card, but I am facing below error in Linux Image. (Alst refer attached SDcard & Sysboot setting in Board)
Linux Version:: Linux-3.2.0
Processor :: AM3358
Error :
U-Boot SPL 2011.09 (Jun 11 2014 - 12:51:27)
Texas Instruments Revision detection unimplemented
No daughter card present
boot_device=8
OMAP_HSMMC1_BASE 1
OMAP SD/MMC: 0
boot mode - FAT
reading u-boot.img
spl_parse_image_header inside if
reading u-boot.img
U-Boot 2011.09 (Jun 11 2014 - 12:51:27)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
No daughter card present
NAND: HW ECC Hamming Code selected
nand_get_flash_type: unknown NAND device: Manufacturer ID: 0x0c, Chip ID: 0x0c
No NAND device found!!!
0 MiB
MMC: OMAP_HSMMC1_BASE 1
OMAP_HSMMC1_BASE 2
OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
Net: cpsw
Hit any key to stop autoboot: 0
SD/MMC found on device 0
reading uEnv.txt
** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage
3163824 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3163760 Bytes = 3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@localhost) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Fri Jun 13 10:14:41 IST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 253256k/253256k available, 8888k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB)
[ 0.000000] .init : 0xc059d000 - 0xc05db000 ( 248 kB)
[ 0.000000] .data : 0xc05dc000 - 0xc0644198 ( 417 kB)
[ 0.000000] .bss : 0xc06441bc - 0xc0671024 ( 180 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.058563] pid_max: default: 32768 minimum: 301
[ 0.058685] Security Framework initialized
[ 0.058776] Mount-cache hash table entries: 512
[ 0.059143] CPU: Testing write buffer coherency: ok
[ 0.079040] omap_hwmod: pruss: failed to hardreset
[ 0.080139] print_constraints: dummy:
[ 0.080505] NET: Registered protocol family 16
[ 0.082611] OMAP GPIO hardware version 0.1
[ 0.085174] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.087402] omap_i2c.1: alias fck already exists
[ 0.088256] omap2_mcspi.1: alias fck already exists
[ 0.088470] omap2_mcspi.2: alias fck already exists
[ 0.089263] edma.0: alias fck already exists
[ 0.089263] edma.0: alias fck already exists
[ 0.089294] edma.0: alias fck already exists
[ 0.116058] bio: create slab <bio-0> at 0
[ 0.118255] SCSI subsystem initialized
[ 0.119934] usbcore: registered new interface driver usbfs
[ 0.120239] usbcore: registered new interface driver hub
[ 0.120452] usbcore: registered new device driver usb
[ 0.120605] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.120880] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.138610] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.140533] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.142913] print_constraints: VRTC:
[ 0.144378] print_constraints: VIO: at 1500 mV
[ 0.146667] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.148986] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.149993] print_constraints: VDD3: 5000 mV
[ 0.151397] print_constraints: VDIG1: at 1800 mV
[ 0.152801] print_constraints: VDIG2: at 1800 mV
[ 0.154235] print_constraints: VPLL: at 1800 mV
[ 0.155639] print_constraints: VDAC: at 1800 mV
[ 0.157073] print_constraints: VAUX1: at 1800 mV
[ 0.158508] print_constraints: VAUX2: at 3300 mV
[ 0.159942] print_constraints: VAUX33: at 3300 mV
[ 0.161346] print_constraints: VMMC: at 3300 mV
[ 0.161865] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.163085] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.164215] Switching to clocksource gp timer
[ 0.179595] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.179779] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.180084] MUSB0 controller's USBSS revision = 4ea20800
[ 0.180664] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18
[ 0.180816] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.181121] MUSB1 controller's USBSS revision = 4ea20800
[ 0.181243] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.181304] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.181457] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.181457] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.181457] usb usb1: Product: MUSB HDRC host driver
[ 0.181488] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.181488] usb usb1: SerialNumber: musb-hdrc.1
[ 0.182250] hub 1-0:1.0: USB hub found
[ 0.182281] hub 1-0:1.0: 1 port detected
[ 0.182800] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19
[ 0.183227] NET: Registered protocol family 2
[ 0.183410] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.183715] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.183868] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.183959] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.183990] TCP reno registered
[ 0.183990] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.184020] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.184173] NET: Registered protocol family 1
[ 0.184539] RPC: Registered named UNIX socket transport module.
[ 0.184539] RPC: Registered udp transport module.
[ 0.184539] RPC: Registered tcp transport module.
[ 0.184570] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.184814] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.196044] VFS: Disk quotas dquot_6.5.2
[ 0.196136] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.196655] msgmni has been set to 494
[ 0.199798] alg: No test for stdrng (krng)
[ 0.200439] io scheduler noop registered
[ 0.200469] io scheduler deadline registered
[ 0.200531] io scheduler cfq registered (default)
[ 0.201690] Could not set LED4 to fully on
[ 0.203460] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.822387] console [ttyO0] enabled
[ 0.826660] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.834442] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.842254] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.850067] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.857849] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.874938] brd: module loaded
[ 0.882995] loop: module loaded
[ 0.886505] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.892944] i2c-core: driver [tsl2550] using legacy resume method
[ 0.899383] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.964813] No daughter card found
[ 0.968383] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.983581] Board name: A335X_SK
[ 0.986938] Board version: 1.2B
[ 0.990234] The board is a AM335x Starter Kit.
[ 0.995117] omap_hsmmc.0: alias fck already exists
[ 1.000640] omap_hsmmc.1: alias fck already exists
[ 1.006683] da8xx_lcdc.0: alias fck already exists
[ 1.012145] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel
[ 1.027435] Console: switching to colour frame buffer device 60x34
[ 1.040252] davinci-mcasp.1: alias fck already exists
[ 1.046173] Configure Bluetooth Enable pin...
[ 1.051605] registered am33xx_sr device
[ 1.055877] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator
[ 1.063476] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator
[ 1.091613] lis3lv02d: unknown sensor type 0x87
[ 1.096405] lis3lv02d_i2c: probe of 1-0018 failed with error -22
[ 1.104278] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.111450] omap2-nand driver initializing
[ 1.115936] OneNAND driver initializing
[ 1.121185] CAN device driver interface
[ 1.125213] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.174835] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.181304] davinci_mdio davinci_mdio.0: detected phy mask fffffffc
[ 1.189514] davinci_mdio.0: probed
[ 1.193084] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.200439] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.208160] usbcore: registered new interface driver zd1201
[ 1.214172] usbcore: registered new interface driver cdc_ether
[ 1.220489] usbcore: registered new interface driver cdc_eem
[ 1.226593] usbcore: registered new interface driver dm9601
[ 1.232452] cdc_ncm: 04-Aug-2011
[ 1.235992] usbcore: registered new interface driver cdc_ncm
[ 1.241882] Initializing USB Mass Storage driver...
[ 1.247222] usbcore: registered new interface driver usb-storage
[ 1.253479] USB Mass Storage support registered.
[ 1.258789] mousedev: PS/2 mouse device common for all mice
[ 1.265716] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0
[ 1.273925] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 1.280609] omap_rtc: already running
[ 1.284606] i2c /dev entries driver
[ 1.288665] Linux video capture interface: v2.00
[ 1.293792] usbcore: registered new interface driver uvcvideo
[ 1.299804] USB Video Class driver (1.1.1)
[ 1.306091] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.314605] cpuidle: using governor ladder
[ 1.319396] cpuidle: using governor menu
[ 1.328125] omap4_aes_mod_init: loading AM33X AES driver
[ 1.333801] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.340332] omap4_aes_probe: probe() done
[ 1.344726] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.350891] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.362579] omap4_sham_probe: probe() done
[ 1.369262] usbcore: registered new interface driver usbhid
[ 1.375091] usbhid: USB HID core driver
[ 1.379791] usbcore: registered new interface driver snd-usb-audio
[ 1.391326] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator
[ 1.399169] _regulator_get: 1-001b supply DVDD not found, using dummy regulator
[ 1.406860] _regulator_get: 1-001b supply AVDD not found, using dummy regulator
[ 1.414520] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator
[ 1.425079] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[ 1.432891] ALSA device list:
[ 1.436035] #0: AM335X EVM
[ 1.439025] oprofile: hardware counters not available
[ 1.444274] oprofile: using timer interrupt.
[ 1.448760] nf_conntrack version 0.5.0 (3957 buckets, 15828 max)
[ 1.455535] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.461181] TCP cubic registered
[ 1.464569] NET: Registered protocol family 17
[ 1.469238] can: controller area network core (rev 20090105 abi 8)
[ 1.475769] NET: Registered protocol family 29
[ 1.480407] can: raw protocol (rev 20090105)
[ 1.484863] can: broadcast manager protocol (rev 20090105 t)
[ 1.490783] Registering the dns_resolver key type
[ 1.495788] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.503784] ThumbEE CPU extension supported.
[ 1.508331] mux: Failed to setup hwmod io irq -22
[ 1.513824] Power Management for AM33XX family
[ 1.518707] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.525360] Copied the M3 firmware to UMEM
[ 1.529815] Compensating OPP0 for 0mV Orig nvalue:0x99c3b2 New nvalue:0x99c3b2
[ 1.537475] Compensating OPP1 for 0mV Orig nvalue:0x998e80 New nvalue:0x998e80
[ 1.549255] Compensating OPP0 for 0mV Orig nvalue:0x99bbae New nvalue:0x99bbae
[ 1.556915] Compensating OPP1 for 0mV Orig nvalue:0x999b8c New nvalue:0x999b8c
[ 1.564514] Compensating OPP2 for 0mV Orig nvalue:0xaae6d1 New nvalue:0xaae6d1
[ 1.572143] Compensating OPP3 for 0mV Orig nvalue:0xaacbb8 New nvalue:0xaacbb8
[ 1.579833] create_regulator: VDD1: Failed to create debugfs directory
[ 1.588195] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.602996] clock: disabling unused clocks to save power
[ 1.621582] Detected MACID=1c:ba:8c:e8:66:a7
[ 1.627166] cpsw: Detected MACID = 1c:ba:8c:e8:66:a9
[ 1.634307] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[ 1.642028] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:48:09 UTC (946687689)
[ 1.651184] Waiting for root device /dev/mmcblk0p2...
[ 1.666473] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 3.042480] mmc0: error -110 whilst initialising SD card
[ 5.045562] Unable to handle kernel paging requect at virtual address fffffffe
[ 5.053100] pgd = c0004000
[ 5.055908] [fffffffe] *pgd=8fffe821, *pte=00000000, *ppte=00000000
[ 5.062500] Internal error: Oops - undefined instruction: 0 [#1]
[ 5.068756] Modules linked in:
[ 5.071929] CPU: 0 Not tainted (3.2.0 #1)
[ 5.076507] PC is at do_timer+0x11c/0x9ac
[ 5.080688] LR is at 0x0
[ 5.083312] pc : [<c005ffd8>] lR : [<00000000>] p3r: 20000193
[ 5.083312] sp : cf951930 ip : 000035cd fp : cf9519c4
[ 5.095275] r10: c05ffe48 r9 : 00000233 r8 : 00000233
[ 5.100738] r7 : 00000007 r6 : c06571e0 r5 : 000071e0 r4 : c0657278
[ 5.107543] r3 : 00000038 r2 : 00989680 r1 : 00000001 r0 : 00000148
[ 5.114349] Flags: nzCv IRQs off FIQc on Mode SVC_32 ISA ARM Segment kernel
[ 5.122039] Control: 10c5387d Table: 80004019 DAC: 00000015
[ 5.128021] Process kworker/0:1 (pid: 417, stack limit = 0xcf9502f0)
[ 5.134643] Stack: (0xcf951930 to 0xcf952000)
[ 5.139190] 1920: fbbff587 fdff1e4f dfff'e3f ffff695d
[ 5.147735] 1940: efff37bd dfdf42fa efdf7d7f fdd7f7f3 00000001 c0657278 bdffce9e fffd3cca
[ 5.156250] 1960: fbefded3 9bfffdbd ef7d55f1 f3dffff4 bffffc24 ffee9faf 0000 233 00000000
[ 5.164794] 1980: ffff5beb ffffaffe fffd6773 fbbfbabc 00000148 00000000 c005f60c c06573e0
[ 5.173309] 19a0: c06573d0 c0657248 00000000 00989680 00000000 c05ffe48 cf9519f4 cf9519c8
[ 5.181823] 19c0: c00658bc c005fec8 c05ffe84 c0600370 2d6bdcc1 00000001 c060 370 cf951b68
[ 5.190368] 19e0: 00000000 00000001 cf951a24 cf9519f8 c0065af8 c006582c c005a4b4 c01d5684
[ 5.198883] 1a00: 2d6bdcc1 00000001 c0600370 c05ffe78 c05ffe48 c05ffe48 cf951a3c cf951a28
[ 5.207427] 1a20: c005a60c c0065a44 2d6bdcc1 00000001 cf951a9c cf951a40 c005aeb8 c005a5d8
[ 5.215942] 1a40: 2d6bdcc1 00000001 2d6bdcc1 00000001 fa30e000 00000000 00000000 00000000
[ 5.224487] 1a60: ffffffff 7fffffff 2d6bdcc1 00000001 00000000 c05e4380 00000044 00000000
[ 5.233001] 1a80: 00000000 00000044 c0657cbc c0602454 cf951aac cf951aa0 c0021ed0 c005add8
[ 5.241546] 1aa0: cf951ae4 cf951ab0 c007202c c0021ea8 cf990800 c06496df 00000001 c0602454
[ 5.250061] 1ac0: 00000044 00000000 cf951b68 f2000000 c0013f28 cf950000 cf951afc cf951ae8
[ 5.258575] 1ae0: c00721a8 c0071fe0 00020000 c0602454 cf951b14 cf951b00 c00740c4 c0072184
[ 5.267120] 1b00: c0074038 c06192c4 cf951b24 cf951b18 c007191c c0074044 cf951b44 cf951b28
[ 5.275634] 1b20: c0015164 c00718f0 00000002 00000004 fa200000 00000044 cf95!b64 cf951b48
[ 5.284179] 1b40: c00085b8 c0015130 c000e950 60000113 ffffffff cf951c9c cf95!c04 cf951b68
[ 5.292694] 1b60: c0013ec0 c0008540 f30e30b4 cf951da0 c0076afc c003e2c0 c05e2190 60000193
[ 5.301239] 1b80: c0014188 00000001 f2000000 c0013f28 cf950000 cf951c04 cf951c08 cf951bb0
[ 5.309753] 1ba0: c0013f20 c000e950 60000113 ffffffff c05004c8 cf951da0 80000007 cf951c18
[ 5.318298] 1bc0: cf951da0 cf950000 c05004c8 80000007 00000000 00100100 cf8a4bc0 cf951c04
[ 5.326812] 1be0: cf951c08 cf951bf8 c003e2c0 c0076afc 60000193 ffffffff cf951c14 cf951c08
[ 5.335357] 1c00: c003e2c0 c0076af8 cf951c94 cf951c18 c0017b6c c003e2bc 00000004 0005bd1c
[ 5.343872] 1c20: cf8a4bc0 000001ff 00000000 cfffe7fc 80000007 00000000 00100100 cf8a4bc0
[ 5.352416] 1c40: cf951c64 cf951c50 c0422544 c003ec00 80000007 cf951c6c cf951c94 cf951c78
[ 5.360931] 1c60: c001a234 c042252c c051bb58 cf951da0 fffffffe 00000000 80000007 00000000
[ 5.369445] 1c80: 00100100 cf8a4bc0 cf951cbc cf951c98 c001a2f4 c0017b4c cf951da0 00000000
[ 5.377990] 1ca0: cf951da0 fffffffe cf951da0 80000007 cf951cf4 cf951cc0 c001a458 c001a284
[ 5.386505] 1cc0: cf951cdc cf951cd0 c0050b6c 00000007 c05e272c fffffffe cf951da0 f0001e24
[ 5.395050] 1ce0: 00100100 00000000 cf951d9c cf951cf8 c0008448 c001a310 c02348ec c02346ac
[ 5.403564] 1d00: 00000001 cf891800 cf951d64 cf951d18 c02d5390 c02349b8 cf=5!dbf cf891840
[ 5.412109] 1d20: cf951dc7 cf8b3e00 cf891840 00000001 c05ff608 00000001 c05f0608 c063c620
[ 5.420623] 1d40: cf951d64 cf951d50 c002ee3c c002ed9c a0000093 000000b7 cf951d7c cf951d68
[ 5.429168] 1d60: c003429c c002ed9c c063be70 c05f7ae8 cf951d94 cf951d80 c002359c c003424c
[ 5.437683] 1d80: fffffffe a00001b3 ffffffff cf951dd4 cf951efc cf951da0 c0013f78 c0008414
[ 5.446228] 1da0: cf951ef0 838d00c0 c0865ac0 cf9d6140 c064430c 00000000 c05e1518 c0657e7c
[ 5.454742] 1dc0: f0001e24 00100100 00000000 cf951efc c0001a80 cf951de8 cf951ffc fffffffe
[ 5.463287] 1de0: a00001b3 ffffffff cf951ef0 838d00c0 c0865ac0 cf9d6140 c064$30c 00000000
[ 5.471801] 1e00: c05e1518 c0657e7c f0001e6c 00100100 00000000 cf951efc c0001a80 00000000
[ 5.480316] 1e20: 00000000 c001435c 00000001 cf94cd98 00000080 838d00c0 c0865ac0 cf9d6140
[ 5.488861] 1e40: c064430c 00000000 c05e1518 c0657e7c f0001eb4 00100100 00000000 cf951efc
[ 5.497375] 1e60: c0001a80 00000000 00000000 c001435c cf951f0c cf951e80 00000080 838d00c0
[ 5.505920] 1e80: c0865ac0 cf9d6140 c064430c 00000000 c05e1518 c0657e7c 00000080 00100100
[ 5.514434] 1ea0: 00000000 cf951efc cf800d90 00000000 00000000 c001435c 00000001 cf8a4d18
[ 5.522979] 1ec0: c060bcb8 00000000 00000004 00200200 c0039f08 cf807e80 00000004 cf807e90
[ 5.531494] 1ee0: c05ff608 c05ff608 c060bfb8 00000000 cf951f1c cf951f00 c00a58e8 c00a53f0
[ 5.540039] 1f00: 00000000 cf800d40 cf802bc0 c06587d0 cf951f4c cf951f20 c00a598c c00a5864
[ 5.548553] 1f20: 60000013 cf8d1280 cf814800 cf950000 00000000 c00a590c c060bfb8 cf814805
[ 5.557098] 1f40: cf951f84 cf951f50 c0050de8 c00a5918 c05ffb70 cf8d1290 c0656d68 cf8d1280
[ 5.565612] 1f60: c05ffb70 cf8d1290 c0656d68 cf950000 00000009 c05ffb6c cf951fbc cf951f88
[ 5.574157] 1f80: c0052c60 c0050cd0 cf8d1280 c0052b04 00000013 cf833ee0 cf8d1280 c0052b04
[ 5.582672] 1fa0: 00000013 00000000 00000000 00000000 cf951ff4 cf951fc0 c0056c78 c0052b10
[ 5.591186] 1fc0: cf833ee0 00000000 cf8d1280 00000000 cf951fd0 cf951fd0 00000000 cf833ee0
[ 5.599731] 1fe0: c0056be8 c00413d4 00000000 cf951ff8 c00413d4 c0056bf4 bffffd8f fffff03b
[ 5.608245] Backtrace:
[ 5.610809] [<c005febc>] (do_timer+0x0/0x9ac) from [<c00658bc>] (tick_do_update_jiffies64+0x9c/0x10c)
[ 5.620452] [<c0065820>] (tick_do_update_jiffies64+0x0/0x10c) from [<c0065af8>] (tick_sched_timer+0xc0/0xc4)
[ 5.630676] r9:00000001 r8:00000000 r7:cf951b68 r6:c0600370 r5:00000001
[ 5.637512] r4:2d6bdcc1
[ 5.640258] [<c0065a38>] (tick_sched_timer+0x0/0xc4) from [<c005a60c>] (__run_hrtimer.clone.33+0x40/0xe8)
[ 5.650238] r7:c05ffe48 r6:c05ffe48 r5:c05ffe78 r4:c0600370
[ 5.656158] [<c005a5cc>] (__run_hrtimer.clone.33+0x0/0xe8) from [<c005aeb8>] (hrtimer_interrupt+0xec/0x278)
[ 5.666290] r5:00000001 r4:2d6bdcc1
[ 5.670043] [<c005adcc>] (hrtimer_interrupt+0x0/0x278) from [<c0021ed0>] (omap2_gp_timer_interrupt+0x34/0x3c)
[ 5.680389] [<c0021e9c>] (omap2_gp_timer_interrupt+0x0/0x3c) from [<c007202c>] (handle_irq_event_percpu+0x58/0x1a4)
[ 5.691284] [<c0071fd4>] (handle_irq_event_percpu+0x0/0x1a4) from [<c00721a8>] (handle_irq_event+0x30/0x40)
[ 5.701446] [<c0072178>] (handle_irq_event+0x0/0x40) from [<c00740c4>] (handle_level_irq+0x8c/0x100)
[ 5.710968] r4:c0602454 r3:00020000
[ 5.714721] [<c0074038>] (handle_level_irq+0x0/0x100) from [<c007191c>] (generic_handle_irq+0x38/0x48)
[ 5.724395] r4:c06192c4 r3:c0074038
[ 5.728149] [<c00718e4>] (generic_handle_irq+0x0/0x48) from [<c0015164>] (handle_IRQ+0x40/0x8c)
[ 5.737243] [<c0015124>] (handle_IRQ+0x0/0x8c) from [<c00085b8>] (omap3_intc_handle_irq+0x84/0x88)
[ 5.746582] r6:00000044 r5:fa200000 r4:00000004 r3:00000002
[ 5.752502] [<c0008534>] (omap3_intc_handle_irq+0x0/0x88) from [<c0013ec0>] (__irq_svc+0x40/0x60)
[ 5.761749] Exception stack(0xcf951b68 to 0xcf951bb0)
[ 5.766998] 1b60: f30e30b4 cf951da0 c0076afc c003e2c0 c05e2190 60000193
[ 5.775543] 1b80: c0014188 00000001 f2000000 c0013f28 cf950000 cf951c04 cf951c08 cf951bb0
[ 5.784057] 1ba0: c0013f20 c000e950 60000113 ffffffff
[ 5.789337] r7:cf951b9c r6:ffffffff r5:60000113 r4:c000e950
[ 5.795257] [<c0076aec>] (tracing_off+0x0/0x30) from [<c003e2c0>] (oops_enter+0x10/0x1c)
[ 5.803710] [<c003e2b0>] (oops_enter+0x0/0x1c) from [<c0017b6c>] (die+0x2c/0x2d8)
[ 5.811523] [<c0017b40>] (die+0x0/0x2d8) from [<c001a2f4>] (flush_cache_range+0x7c/0x8c)
[ 5.819946] [<c001a278>] (flush_cache_range+0x0/0x8c) from [<c001a458>] (flush_cache_page+0x154/0x1f0)
[ 5.829650] r8:80000007 r7:cf951da0 r6:fffffffe r5:cf951da0 r4:00000000
[ 5.836456] r3:cf951da0
[ 5.839202] [<c001a304>] (flush_cache_page+0x0/0x1f0) from [<c0008448>] (do_PrefetchAbort+0x40/0xa4)
[ 5.848724] [<c0008408>] (do_PrefetchAbort+0x0/0xa4) from [<c0013f78>] (__pabt_svc+0x38/0x80)
[ 5.857635] Exception stack(0xcf951da0 to 0xcf951de8)
[ 5.862884] 1da0: cf951ef0 838d00c0 c0865ac0 cf9d6140 c064430c 00000000 c05e1518 c0657e7c
[ 5.871429] 1dc0: f0001e24 00100100 00000000 cf951efc c0001a80 cf951de8 cf951ffc fffffffe
[ 5.879943] 1de0: a00001b3 ffffffff
[ 5.883575] r7:cf951dd4 r6:ffffffff r5:a00001b3 r4:fffffffe
[ 5.889495] [<c00a53e4>] (flush_old_exec+0x0/0x170) from [<c00a58e8>] (check_unsafe_exec+0x90/0xb4)
[ 5.898925] [<c00a5858>] (check_unsafe_exec+0x0/0xb4) from [<c00a598c>] (do_execve+0x80/0x124)
[ 5.907928] r6:c06587d0 r5:cf802bc0 r4:cf800d40 r3:00000000
[ 5.913848] [<c00a590c>] (do_execve+0x0/0x124) from [,c0050de8>] (process_one_work+0x124/0x384)
[ 5.922912] [<c0050cc4>] (process_one_work+0x0/0x384) from [<c0052c60>] (worker_thread+0x15c/0x330)
[ 5.932342] [<c0052b04>] (worker_thread+0x0/0x330) from [<c0056c78>] (kthread+0x90/0x94)
[ 5.940795] [<c0056be8>] (kthread+0x0/0x94) from [<c00413d4>] (do_exit+0x0/0x67c)
[ 5.948608] r6:c00413d4 r5:c0056be8 r4:cf833ee0
[ 5.953430] Code: e16f3f12 e2633040 e30751e0 e263703f (f34c5065)
Please help me out from this...
Thanks in advance...
Ankur