HI,
I want to use in the disable the RTC of AM335x.
I am using the TPS65910 as PMIC.
It becomes the connection, such as the following in TMDXEVM3358.
PWRON : open
PWRHOLD : PMIC_POWER_EN(AM335x output)
*I believe that it is not available when PMIC_POWER_EN you have to disable the RTC.
You are connected to the +5 V PWRHOLD pin in order to activate the TPS65910A after turning of +5 V According to an article in the E2E below.
TI E2E Community
TMDSSK3358 automatic boot upon power-up
http://e2e.ti.com/support/arm/sitara_arm/f/791/p/235319/851516.aspx#851516
What do I need to connect to PWRHOLD Pin? Sure you want a +5 V?
Best Regards,
hamada