This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about interlace video encode in DVRRDK 3.0?

Hello,TIer.
 I'm using DM8168, with RDK 3.0.
  In my usecase, the resolution of SWMS is 1080P30, I want to encode it into 2-H264- channel, one with  480i50, the other with 1080i50 or 720p25;
  Scalar LINK can be adopted following SWMS LINK to scale the channel from 1080p30 to 480p30, then delivered to EncoderLINK;
  But the input of the EncoderLINK is progressive, can it generate interleaving h264 stream, and how to set?
 Or,Could scaler generate interlace video?
  The output framerate of EncoderLINK is not identical with the input, can it work properly? 
BR!