Hi, All,
we designed our custom board based on the dm8168 with HDCP support, everything seems fine expect the analog video DAC, we used the same power regulator TPS65001 as the EVM for the 1.8V analog input, and the current of this power rail is around 60mA when the board is running, for couple of our boards, the processor seems short inside on the VDAC side after couple days runing, cause the load for the 1.8V analog is small which short theTPS65001, and the power chip got so hot, which prevent the board boot into system successfully~~ we replaced the power regular, and it performed the same, the internel load for the 1.8V analog is 2ohm when power down., for the good board, the load is close to 2K ohm/
Anyoen has clue on this, we still trying to figue out this problem,