Other Parts Discussed in Thread: SN74LVCH16245A
Sir,
I am using TMS320C6211 based custom board. In my project i am using EMIF CE2 space for both reading and writng. I can read from EMIF CE2 asynchronous memory. But when i writng to the memory is not working unless i manually put the AWE pin of EMIF to the ground. (is not a good practice since AWE automatically changes its logic while reading and writing)
I am using sn74lvch16245a transceiver ic, data lines from dsp connected to B port, AWE pin connected to DIR pin of transceiver ic, if AWE pin is low, then output is obtained from A port.(As per sn74lvch1625a datasheet)
I checked the status of AWE pin, it is always showing 2.19V.
What will be the defualt value of AWE pin? or Is it due to my board not properly grounded?
can anyone help me ?