Other Parts Discussed in Thread: OMAPL138, OMAP-L138, DA8XX, PMP, ADS7846
Hi TI E2E Community,
I am now using OMAPL138 evaluation board for our project. Now I have run the syslink_2_21_03_11 ex02_messageq examples.when dsp and host are running,I enter "CTRL+C" to force the host process to exit and then the linux kernel was aborted.Here are some exception information:
root@omapl138-lcdk:/ex02_messageq/release# ./run.sh
+ ./slaveloader startup DSP server_dsp.xe674
Attached to slave procId 0.
Loading procId 0.
Loaded file server_dsp.xe674 on slave procId 0.
Started slave procId 0.
+ ./app_host DSP
--> main:
--> Main_main:
--> App_create:
^C[ 84.519119] *** Platform_stopCallback: Ipc_stop timeout - Ipc_stop not called by slave?
[ 84.519148] Error [0xffffffff] at Line no: 2366 in file /home/hxd/omapl138/syslink_2_21_03_11/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/family/hlos/knl/omapl1xx/Platform.c
[ 84.551227] *** _Notify_unregisterEventSingle: Notify driver not registered
[ 84.551255] Error [0xfffffff9] at Line no: 1413 in file /home/hxd/omapl138/syslink_2_21_03_11/packages/ti/syslink/utils/hlos/knl/Linux/../../../../../../ti/syslink/ipc/hlos/knl/Notify.c
[ 84.577306] Unable to handle kernel paging request at virtual address c9df2038
[ 84.585536] pgd = c0004000
[ 84.588332] [c9df2038] *pgd=c68d7811, *pte=00000000, *ppte=00000000
[ 84.595606] Internal error: Oops: 7 [#1] PREEMPT
[ 84.600263] Modules linked in: syslink(O) ipv6 minix
[ 84.605313] CPU: 0 Tainted: G O (3.3.0 #2)
[ 84.611329] PC is at GateMP_enter+0x28/0xa0 [syslink]
[ 84.617047] LR is at GateMP_enter+0x28/0xa0 [syslink]
[ 84.622153] pc : [<bf097844>] lr : [<bf097844>] psr: 80000013
[ 84.622170] sp : c689fd10 ip : 00000000 fp : c689fd24
[ 84.633712] r10: 00000000 r9 : c780de70 r8 : 00000001
[ 84.638975] r7 : c9e37000 r6 : bf13c238 r5 : c9e3500c r4 : c9df2000
[ 84.645550] r3 : c9df2000 r2 : bf0f238f r1 : c9df2000 r0 : bf0f238f
[ 84.652125] Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 84.659315] Control: 0005317f Table: c6844000 DAC: 00000015
[ 84.665107] Process app_host (pid: 1172, stack limit = 0xc689e270)
[ 84.671334] Stack: (0xc689fd10 to 0xc68a0000)
[ 84.675734] fd00: 00000000 c9e39000 c689fd54 c689fd28
[ 84.683988] fd20: bf09f29c bf09782c bf072588 bf0715a8 00000494 c8b30000 00000000 c018f355
[ 84.692240] fd40: c683da08 00000000 c689fd74 c689fd58 bf0d3ca4 bf09f128 00000000 c018f355
[ 84.700494] fd60: c683da08 00000494 c689fd9c c689fd78 bf0d3dec bf0d3ca0 c68a0170 c9e35000
[ 84.708752] fd80: c683da00 c68a0170 c7552e00 00000008 c689fdd4 c689fda0 c008e2d8 bf0d3d90
[ 84.717004] fda0: 00000000 00000000 ffffffff c683da00 00000000 c7189c00 c73c1f20 00000038
[ 84.725258] fdc0: c689ffb0 00000000 c689fdf4 c689fdd8 c008ab5c c008e1d4 c7083838 c7189c00
[ 84.733509] fde0: 00000000 0000003f c689fe1c c689fdf8 c001b3f4 c008aaf4 c7189c00 00000002
[ 84.741764] fe00: 00418004 c689fec8 c70bdf64 c71c7c00 c689fe34 c689fe20 c001b504 c001b380
[ 84.750016] fe20: 00000000 c72f6580 c689fe64 c689fe38 c001b704 c001b4b8 c00258b0 00000001
[ 84.758269] fe40: 00000000 00000000 00000000 ffffffff bf0ccb70 c689fec8 c689fe7c c689fe68
[ 84.766524] fe60: c001bf88 c001b518 418004fc c689e000 c689feb4 c689fe80 c0027d7c c001bed8
[ 84.774777] fe80: c70bdec0 c689ff48 00000000 c689ffb0 46ce5df0 fffffe00 000000f0 c00095c4
[ 84.783032] fea0: c689e000 46ce5dec c689ff94 c689feb8 c000b348 c002789c c004c134 c004a058
[ 84.791282] fec0: ffffffff 00000000 00000009 00000000 00000000 00000000 00000000 c680fc00
[ 84.799535] fee0: bedb3c1c bedb3c1c c783e170 c00095c4 c689e000 00000000 c689ff7c c689ff08
[ 84.807787] ff00: c009cf90 bf0cb5ec 00000000 00000000 c7114c00 00000010 c7114d88 00000002
[ 84.816039] ff20: c7389950 00000000 c689e000 00000000 00000000 00000080 0002283c c00095c4
[ 84.824291] ff40: c689e000 00000000 c689ffa4 c689ff58 c004cc48 c004c0a0 b6fb5870 00000000
[ 84.832542] ff60: ffffffff c00095c4 c689e000 00000001 0002283c 00000000 000000f0 00000000
[ 84.840796] ff80: c689e000 00000000 c689ffac c689ff98 c000bd5c c000b28c 00000001 b6fb5870
[ 84.849048] ffa0: 00000000 c689ffb0 c0009494 c000bd4c 0002283c 00000080 00000000 00000000
[ 84.857299] ffc0: b6fb5870 0002283c 00000000 000000f0 00022844 00000000 46afd000 00000000
[ 84.865552] ffe0: 00000000 bedb3c20 46ce5dd8 46ce5dec 80000010 0002283c c7ffe831 c7ffec31
[ 84.873777] Backtrace:
[ 84.877537] [<bf09781c>] (GateMP_enter+0x0/0xa0 [syslink]) from [<bf09f29c>] (HeapBufMP_delete+0x184/0x3f0 [syslink])
[ 84.888229] r4:c9e39000 r3:00000000
[ 84.893192] [<bf09f118>] (HeapBufMP_delete+0x0/0x3f0 [syslink]) from [<bf0d3ca4>] (HeapBufMPDrv_cmd_delete+0x14/0x60 [syslink])
[ 84.906193] [<bf0d3c90>] (HeapBufMPDrv_cmd_delete+0x0/0x60 [syslink]) from [<bf0d3dec>] (HeapBufMPDrv_close+0x6c/0xb4 [syslink])
[ 84.917843] r4:00000494
[ 84.921150] [<bf0d3d80>] (HeapBufMPDrv_close+0x0/0xb4 [syslink]) from [<c008e2d8>] (fput+0x114/0x200)
[ 84.930441] r7:00000008 r6:c7552e00 r5:c68a0170 r4:c683da00
[ 84.936200] [<c008e1c4>] (fput+0x0/0x200) from [<c008ab5c>] (filp_close+0x78/0x84)
[ 84.943871] [<c008aae4>] (filp_close+0x0/0x84) from [<c001b3f4>] (put_files_struct+0x84/0xe0)
[ 84.952454] r6:0000003f r5:00000000 r4:c7189c00 r3:c7083838
[ 84.958214] [<c001b370>] (put_files_struct+0x0/0xe0) from [<c001b504>] (exit_files+0x5c/0x60)
[ 84.966828] [<c001b4a8>] (exit_files+0x0/0x60) from [<c001b704>] (do_exit+0x1fc/0x708)
[ 84.974798] r4:c72f6580 r3:00000000
[ 84.978443] [<c001b508>] (do_exit+0x0/0x708) from [<c001bf88>] (do_group_exit+0xc0/0xec)
[ 84.986587] r7:c689fec8
[ 84.989172] [<c001bec8>] (do_group_exit+0x0/0xec) from [<c0027d7c>] (get_signal_to_deliver+0x4f0/0x56c)
[ 84.998628] r4:c689e000 r3:418004fc
[ 85.002274] [<c002788c>] (get_signal_to_deliver+0x0/0x56c) from [<c000b348>] (do_signal+0xcc/0x5bc)
[ 85.011407] [<c000b27c>] (do_signal+0x0/0x5bc) from [<c000bd5c>] (do_notify_resume+0x20/0x54)
[ 85.020016] [<c000bd3c>] (do_notify_resume+0x0/0x54) from [<c0009494>] (work_pending+0x24/0x28)
[ 85.028773] r4:b6fb5870 r3:00000001
[ 85.032405] Code: e5930000 e59f2068 e1a03004 ebff6754 (e5944038)
[ 85.043782] ---[ end trace c6ba20824e313edc ]---
[ 85.048463] Fixing recursive fault but reboot is needed!
Why the linux kernel was aborted?
Looking forward for your quick reply. My heartfelt thanks in advance to those who all are giving reply for this post.