Other Parts Discussed in Thread: AM3359, TPS65910, DA8XX
Hi ,sir:
I have a custom am3359 board. I porting the SDK6.00.00.00 to it.
Booting the board with SD card, and the filesystem use the arago-base-tisdk-image-am335x-evm.tar.gz
Something wrong with booting. It's halt in starting udev step,why?
my booting log as below.
=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2014.06.18 11:19:42 =~=~=~=~=~=~=~=~=~=~=~=
CCCCCCCC
U-Boot SPL 2013.01.01 (Jun 13 2014 - 01:31:48)
Incorrect magic number (0xffffffff) in EEPROM
Could not get board ID.
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx,
SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx,
SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01 (Jun 13 2014 - 01:31:48)
I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
Incorrect magic number (0xffffffff) in EEPROM
Could not get board ID.
NAND: 512 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx,
SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx,
SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
PHY reset timed out
cpsw, usb_ether
Hit any key to stop autoboot: 5 4 3 2 1 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage ?189856 bytes read in 351 ms (8.7 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3189792 Bytes = 3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (fan@ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-
NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #14 Mon Jun 16 23:33:25 PDT 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3
rootwait ip=none
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry 鉧che hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513180k/513180k available, 11108k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0596000 (5688 kB)
[ 0.000000] .init : 0xc0596000 - 0xc05d1000 ( 236 kB)
[ 0.000000] .data : 0xc05d2000 - 0xc063b3b0 ( 421 kB)
[ 0.000000] .bss : 0xc063b3d4 - 0xc066a1a4 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 25000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000091] Calibrating delay loop... 749.56 BogoMIPS (lpj=3747840)
[ 0.089050] pid_max: default: 32768 minimum: 301
[ 0.089172] Security Framework initialized
[ 0.089263] Mount-cache hash table entries: 512
[ 0.089630] CPU: Testing write buffer coherency: ok
[ 0.109680] omap_hwmod: pruss: failed to hardreset
[ 0.110778] print_constraints: dummy:
[ 0.111145] NET: Registered protocol family 16
[ 0.113189] OMAP GPIO hardware version 0.1
[ 0.115692] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.117431] omap_i2c.1: alias fck already exists
[ 0.118255] omap2_mcspi.1: alias fck already exists
[ 0.118438] omap2_mcspi.2: alias fck already exists
[ 0.119384] edma.0: alias fck already exists
[ 0.119415] edma.0: alias fck already exists
[ 0.119415] edma.0: alias fck already exists
[ 0.145172] bio: create slab <bio-0> at 0
[ 0.147277] SCSI subsystem initialized
[ 0.148834] usbcore: registered new interface driver usbfs
[ 0.149169] usbcore: registered new interface driver hub
[ 0.149353] usbcore: registered new device driver usb
[ 0.149627] registerd cppi-dma Intr @ IRQ 17
[ 0.149658] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.149658] Cppi41 Init Done
[ 0.149688] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.149993] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.151062] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.152832] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.155151] print_constraints: VRTC:
[ 0.156524] print_constraints: VIO: at 1500 mV
[ 0.158721] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.160949] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.161926] print_constraints: VDD3: 5000 mV
[ 0.163269] print_constraints: VDIG1: at 1800 mV
[ 0.164642] print_constraints: VDIG2: at 1800 mV
[ 0.166015] print_constraints: VPLL: at 1800 mV
[ 0.167358] print_constraints: VDAC: at 1800 mV
[ 0.168731] print_constraints: VAUX1: at 1800 mV
[ 0.170135] print_constraints: VAUX2: at 3300 mV
[ 0.171478] print_constraints: VAUX33: at 3300 mV
[ 0.172851] print_constraints: VMMC: at 3300 mV
[ 0.173339] tps65910 1-?2d: No interrupt support, no core IRQ
[ 0.174652] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.175781] Switching to clocksource gp timer
[ 0.190521] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.190704] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.191009] MUSB0 controller's USBSS revision = 4ea20800
[ 0.191894] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
[ 0.192047] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.192352] MUSB1 controller's USBSS revision = 4ea20800
[ 0.192779] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.192840] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.192962] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.192993] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.192993] usb usb1: Product: MUSB HDRC host driver
[ 0.193023] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.193023] usb usb1: SerialNumber: musb-hdrc.1
[ 0.193786] hub 1-0:1.0: USB hub found
[ 0.193817] hub 1-0:1.0: 1 port detected
[ 0.194366] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
[ 0.194793] NET: Registered protocol family 2
[ 0.194976] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.195251] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.195526] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.195709] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.195709] TCP reno registered
[ 0.195739] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.195739] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.196014] NET: Registered protocol family 1
[ 0.196258] RPC: Registered named UNIX socket transport module.
[ 0.196258] RPC: Registered udp transport module.
[ 0.196289] RPC: Registered tcp transport module.
[ 0.196289] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.196533] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.215179] VFS: Disk quotas dquot_6.5.2
[ 0.215240] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.215759] msgmni has been set to 1002
[ 0.218811] alg: No test for stdrng (krng)
[ 0.219482] io scheduler noop registered
[ 0.219512] io scheduler deadline registered
[ 0.219573] io scheduler cfq registered (default)
[ 0.220672] Could not set LED4 to fully on
[ 0.236846] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.854461] console [ttyO0] enabled
[ 0.858551] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.866088] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.873596] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.881103] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.888610] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.896575] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 0.912292] brd: module loaded
[ 0.919982] loop: module loaded
[ 0.923309] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.929565] i2c-core: driver [tsl2550] using legacy resume method
[ 0.935760] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.996368] No daughter card found
[ 0.999847] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.008850] The board is general purpose EVM in profile 0
[ 1.015167] da8xx_lcdc.0: alias fck already exists
[ 1.020507] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 1.038360] Console: switching to colour frame buffer device 100x30
[ 1.051910] omap-gpmc omap-gpmc: GPMC revision 6.0
[ 1.056793] Registering NAND on CS0
[ 1.061035] omap_hsmmc.0: alias fck already exists
[ 1.070312] registered am33xx_sr device
[ 1.076660] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.083618] omap2-nand driver initializing
[ 1.088104] ONFI flash detected
[ 1.091369] ONFI param page 0 valid
[ 1.094879] NAND device: Manufacturer ID: 0xad, Chip ID: 0xdc (Hynix H27U4G8F2DTR-BC)
[ 1.102966] Creating 8 MTD partitions on "omap2-nand.0":
[ 1.108337] 0x000000000000-0x000000020000 : "SPL"
[ 1.114501] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 1.121154] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 1.127777] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.134399] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.141326] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.147918] 0x000000280000-0x000000780000 : "Kernel"
[ 1.156127] 0x000000780000-0x000020000000 : "File System"
[ 1.372100] OneNAND driver initializing
[ 1.377380] CAN device driver interface
[ 1.381225] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.436431] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.442657] davinci_mdio davinci_mdio.0: detected phy mask ffffffef
[ 1.449584] davinci_mdio.0: probed
[ 1.453033] davinci_mdio davinci_mdio.0: phy[4]: device 0:04, driver unknown
[ 1.460479] usbcore: registered new interface driver zd1201
[ 1.466247] usbcore: registered new interface driver cdc_ether
[ 1.472290] usbcore: registered new interface driver cdc_eem
[ 1.478149] usbcore: registered new interface driver dm9601
[ 1.483795] cdc_ncm: 04-Aug-2011
[ 1.487213] usbcore: registered new interface driver cdc_ncm
[ 1.492889] Initializing USB Mass Storage driver...
[ 1.498016] usbcore: registered new interface driver usb-storage
[ 1.504058] USB Mass Storage support registered.
[ 1.509124] mousedev: PS/2 mouse device common for all mice
[ 1.515625] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 1.523895] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.530853] i2c /dev entries driver
[ 1.534729] Linux video capture interface: v2.00
[ 1.539703] usbcore: registered new interface driver uvcvideo
[ 1.545501] USB Video Class driver (1.1.1)
[ 1.587524] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.598175] cpuidle: using governor ladder
[ 1.602783] cpuidle: using governor menu
[ 1.610107] omap4_aes_mod_init: loading AM33X AES driver
[ 1.615570] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.621948] omap4_aes_probe: probe() done
[ 1.626220] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.632171] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.643768] omap4_sham_probe: probe() done
[ 1.650360] usbcore: registered new interface driver usbhid
[ 1.655944] usbhid: USB HID core driver
[ 1.660522] tiadc tiadc: attached adc driver
[ 1.668731] usbcore: registered new interface driver snd-usb-audio
[ 1.676879] ALSA device list:
[ 1.679901] No soundcards found.
[ 1.683319] oprofile: hardware counters not available
[ 1.688415] oprofile: using timer interrupt.
[ 1.692718] nf_conntrack version 0.5.0 (8018 buckets, 32072 max)
[ 1.699340] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.704803] TCP cubic registered
[ 1.708099] NET: Registered protocol family 17
[ 1.712585] can: controller 醨ea network core (rev 20090105 abi 8)
[ 1.718902] NET: Registered protocol family 29
[ 1.723358] can: raw protocol (rev 20090105)
[ 1.727661] can: broadcast manager protocol (rev 20090105 t)
[ 1.733398] Registering the dns_resolver key type
[ 1.738220] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.745941] ThumbEE CPU extension supported.
[ 1.750305] mux: Failed to setup hwmod io irq -22
[ 1.755706] Power Management for AM33XX family
[ 1.760437] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.766876] Copied the M3 firmware to UMEM
[ 1.771057] Cortex M3 Firmware Version = 0x181
[ 1.779998] create_regulator: VDD1: Failed to create debugfs directory
[ 1.788085] smartreflex smartreflex: am33xx_sr_probe: Driver initialized
[ 1.802673] clock: disabling unused clocks to save power
[ 1.820007] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.829864] Detected MACID=78:c5:e5:76:9d:e3
[ 1.835113] mmc0: new high speed SDHC card at address 0007
[ 1.841278] cpsw: Detected MACID = 78:c5:e5:76:9d:e4
[ ?847320] mmcblk0: mmc0:0007 SD4GB 3.67 GiB 奫 1.853851] input: gpio-keys as
/devices/platform/gpio-keys/input/input1
[ 1.861053] mmcblk0: p1 p2
[ 1.864868] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 1.882141] kjournald starting. Commit interval 5 seconds
[ 1.887756] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 1.894714] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 1.901977] Freeing init memory: 236K
INIT: version 2.88 bootingStarting udev ?