When running the Magic Lantern demo locally on the Beaglebone Black some error messages appear like the following:
Can't open keypad input device (/dev/input/event0)
PVRShell: EGL 1.4 initialized
Exit message has been set to: "PVRShell: Unable to create surface
".
InitAPI failed!
PVRShell: Unable to create surface
The Beaglebone Black is running Ubuntu 14.04 LTS with the SGX driver (ver 5.1.0).