Other Parts Discussed in Thread: OMAP3530, ADS7846, SYSCONFIG
Hi, I'm using the 2.6.32 kernel from the PSP release ont eh OMAP3EVM. When the board is booted, i get the below dss message nad the LCD backlight goes off. <4>omap-dss: Could not find exact pixel clock. Requested 25189 kHz, got 25188 kHz omap-dss: Could not find exact pixel clock. Requested 25189 kHz, got 25188 kHz The LCD back light comes only when we hit an "Enter key" on the serial Console. Is there any command to keep the LCD On continously?