Hello TI,
We are investigating booting our C6748-based design from eMMC instead of the 16-bit parallel NOR interface which we have traditionally been using. The latest eMMC parts available support the eMMC v.5 standard and are sized 2GB and up. We run our own SysBios-based OS. We use the SecureBoot versions of the C6748 and thus do not wish to use a Secondary Bootloader in order to avoid booting in the clear.
1) It is not quite apparent whether we could use the eMMC boot option in 8-bit mode. Is this possible?
2) If so, equivalent or better boot speeds might arguably be expected compared to 16-bit NOR boot (both with optimised timing). Our image is approx. 16MB. Does anyone have practical experience here?
3) Any other boot-related issues we should be aware of in the light of the currently available eMMC offering (eg. 2GB limit)?
Regards,
Bernhard