Hi all,
I have few C6654 bootload questions from "KeyStone Architecture DSP Bootloader(sprugy5c.pdf)".
1. What is the "Boot Parameter Table" In the section 3.2 Boot Configuration Format ? is it Device Configuration Pins in C6654 Data Manual?
2. Could you provide an example of "Boot Table" and "Boot Configuration Table" ? As you can see there are some tools to generate the "Boot Table" and "Boot Configuration Table" in section 3.2.4 Utilities Used to Generate Different, please provide the real example for reference.
3. As you can see section 3.12.2 Booting an Image From I2C Into an External DDR Memory Using Boot Config Table & 3.12.3 Booting an Image From I2C Into an External DDR Memory Using DDR EMIF Table. Could we apply it through SPI ?
Thanks in advance.
B.R.
OC