This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power sequence on dm8168



Hi All,

I know the power up order must be followed by data sheet, which is 3.3V > 1V_AVS > 1V_CON > 1.8V > 1.5V > 0.9V, so what is the result if the power up mismatch,  my custom board have 1V_CON  ahead 1V_AVS by 2~3ms,  all the rest are ok, so what will be the potential problem? damage? or something else? thank you in advance!

Kevin