This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with TIViddec2 while playing streamed data on DM6446



Hi,

we are using "gst-ti-plugin-full-1.01.00" version for our development with  dvsdk_2_00_00_22 with mv_pro5 kernal.

Below is the pipeline that we are using to display video on DM6446.

gst-launch --gst-debug-no-color --gst-debug=TI*:5  \
gstrtpbin name=rtpbin \
udpsrc port=9010  \
caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264,payload=126" ! \
rtpbin.recv_rtp_sink_0  rtpbin. !   \
rtph264depay ! typefind ! \
TIViddec2 genTimeStamps=FALSE engineName=encodedecode codecName=h264dec displayBuffer=TRUE numOutputBufs=1 ! TIDmaiVideoSink displayStd=v4l2 displayDevice=/dev/video2 videoStd=D1_NTSC videoOutput=COMPOSITE resizer=FALSE accelFrameCopy=FALSE  contiguousInputFrame=TRUE qos=false  sync=false

Video is streamed over UDP from PC.

The following are things that I observerd while playing Video on DM6446.

1. It takes almost one to 2  minute to start playing the video, and 2 min delay in playing live video.

 after some time system will be totally hung and only way to recover from this is to do reboot.

2.One more thing I observed is when the EVM is switched on the if we run the display script, nothing will be diplayed, after trying for 3 to 4 times continously with out changing anything in the pipeline, I could able to see the display.

please let me know how to get the smoth video play with TIViddec2.

In the forums I have observed the following lines added to the caps filter

"profile-level-id=(string)42801e, sprop-parameter-sets=(string)\"Z0KAHtoC0PRA\\,aM48gA\\=\\=\", payload=(int)96, ssrc=(guint)2285223252, clock-base=(guint)1618245704, seqnum-base=(guint)10023"

I tried adding the aboove lines to the pipeline. but I got error.What is the significance of this

Please help us to resolve this issue

Thanks

Deepthi Kiran