This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual Video input support for DM8168

In My design, Ports VIN0 should support 24 bit format and VIN1 should support 16  bit format video input. The signal list is attached.Please let me know whether the signals used are correct?, for port VIN1, HSYNC and VSYNC are pin multiplexed with VIN[0]A_D[16] and VIN[0]A_D[17]. So for port VIN[1] which are the pins to be used for HSYNC and VSYNC? Please clarify.

Video input signals.pdf