This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSI-2 Camera interface

Plz. comment on whether OMAP5 EVM supports 4-lane and 2-lane dual LVDS camera interface.

Also hOW can I get the full technical datasheet of the processor .

  • Hi Abhishek,

    OMAP5 EVM has only MIPI CSI connectors. The two camera expansion connectors are:

    J2 - 30-pin Single CSI Camera Expansion Connector

    J18 - 60-pin Dual-CSI/Parallel Camera Expansion Connector

    If you want to connect LVDS sensor to either of the above listed interfaces, you will need LVDS to CSI converter (either it should be integrated in sensor SOC, or separate device as bridge between the CSI interface & the sensor). See the following e2e threads for pointers:

    http://e2e.ti.com/support/interface/digital_interface/f/130/t/258220.aspx

    http://e2e.ti.com/support/omap/f/849/t/282430.aspx

    Here are the publicly available OMAP5 documents (Technical Reference Manual, Data Manual, Errata and Application Notes): http://www.ti.com/product/omap5432

    For NDA versions of the TRM & DM you should contact your local FAE to provide them.

    Best Regards,
    Yordan