Hello,
I am working on project using ezdpsC5535 and Connected audio framework 02.00.02.04.
My goal is to stream audio to I2S0 port acting as master. Unfortunately when
i2sTxConfig.i2sMode and i2sRxConfig.i2sMode are switched from SLAVE to MASTER
bout Windows and Ubuntu PC stop recognizing C5535 as valid USB audio device (it is detected
but can not be used for audio in or out).
I2S0 CLK and FS are outputted as expected but there is no tx audio data.
Thanks in advance for your replay.
Best regards,
Predrag Milicevic.