Hi,
I noticed TI released the new chip for ADAS as well as the TI Vision SDK.
The Vision SDK is compatible with c64x+, c674 DSP cores (if I am correct). So I am wondering if this SDK is available for DM8148 users.
Thanks a lot.
Yuanwei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I noticed TI released the new chip for ADAS as well as the TI Vision SDK.
The Vision SDK is compatible with c64x+, c674 DSP cores (if I am correct). So I am wondering if this SDK is available for DM8148 users.
Thanks a lot.
Yuanwei
Hi Yuanwei,
Yes, I think we have Vision SDK for DM814x device, see the below links:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/262040.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/325470.aspx
http://e2e.ti.com/support/embedded/tirtos/f/355/t/325754.aspx
But this Vision SDK is not freely available to download from the TI website. You should contact your local FAE / TI representative.
The freely available DM814x software is at the below link:
http://www.ti.com/product/TMS320DM8148/toolssoftware - TI-RTOS, EZSDK, DSPLIB and IMGLIB
Regards,
Pavel
Pavel,
Thank you so much for all the references.
I will contact our local FAE for further information.
Best,
Yuanwei
Hi ,
Trying to build Vision SDK linux version, but i am not able to build and getting following error
# Invoking configuro...
/home/saravana/VISION_SDK_02_02_01_00/ti_components/os_tools/linux/xdctools_3_25_05_94/xs: 45: exec: /home/saravana/VISION_SDK_02_02_01_00/ti_components/os_tools/linux/xdctools_3_25_05_94/xs.x86U: not found
make[3]: *** [xdc_configuro] Error 127
make[2]: *** [apps] Error 2
make[1]: *** [examples] Error 2
make: *** [vision_sdk_examples] Error 2
please help
Hello Saravanakumar Arthanarisami ,
Do you have the tools for linux...?
The release VISION_SDK_02_02_01_00 doesn't have linux tools packaged .
You can contact local FAE for the tools or get the latest release vision_sdk_02_03_00_00 for linux.
Regards
Chetan.M