Hello All,
I am currently using DM365EVM to interface with our sensor and currently we are doing schematics for the sensor board.
As per the dm365 datasheet, the image sensor interface data pins, sync signals have supply voltage of Vdd_isif18_33 (switchable 1.8V/3.3V).
I would like to know where the selection is made between 1.8V and 3.3V.
Is there any jumper/register setting on the EVM or it is upto to the user to connect suitable voltage (1.8V/3.3V) as per his requirement?
Please clarify.
--
Best Regards
Arun