Other Parts Discussed in Thread: TPS65910, DA8XX
Hi,
I am facing the Linux kernel booting issue in AM335 customized board.
Please see the below Customize board log:
U-Boot SPL 2011.09 (Jun 20 2014 - 14:52:20)
Texas Instruments Revision detection unimplemented
### Use AM335x_SK V1.2 setting ###
No daughter card present
boot_device=8
OMAP_HSMMC1_BASE 1
OMAP SD/MMC: 0
boot mode - FAT
reading u-boot.img
spl_parse_image_header inside if
reading u-boot.img
U-Boot 2011.09 (Jun 20 2014 - 14:52:20)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
### Use AM335x_SK V1.2 setting ### Lnt
No daughter card present
NAND: HW ECC Hamming Code selected
No NAND device found!!!
0 MiB
MMC: OMAP_HSMMC1_BASE 1
OMAP_HSMMC1_BASE 2
OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
Net: cpsw
Hit any key to stop autoboot: 0
SD/MMC found on device 0
reading uEnv.txt
** Unable to read "uEnv.txt" from mmc 0:1 **
reading uImage
3164024 bytes read
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3163960 Bytes = 3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@localhost) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Fri Jun 20 16:28:28 IST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 253256k/253256k available, 8888k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059e000 (5720 kB)
[ 0.000000] .init : 0xc059e000 - 0xc05dc000 ( 248 kB)
[ 0.000000] .data : 0xc05dc000 - 0xc0644198 ( 417 kB)
[ 0.000000] .bss : 0xc06441bc - 0xc0671024 ( 180 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.058532] pid_max: default: 32768 minimum: 301
[ 0.058654] Security Framework initialized
[ 0.058746] Mount-cache hash table entries: 512
[ 0.059143] CPU: Testing write buffer coherency: ok
[ 0.079040] omap_hwmod: pruss: failed to hardreset
[ 0.080108] print_constraints: dummy:
[ 0.080474] NET: Registered protocol family 16
[ 0.082550] OMAP GPIO hardware version 0.1
[ 0.085113] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.087310] omap_i2c.1: alias fck already exists
[ 0.088165] omap2_mcspi.1: alias fck already exists
[ 0.088378] omap2_mcspi.2: alias fck already exists
[ 0.089172] edma.0: alias fck already exists
[ 0.089202] edma.0: alias fck already exists
[ 0.089202] edma.0: alias fck already exists
[ 0.115661] bio: create slab <bio-0> at 0
[ 0.117858] SCSI subsystem initialized
[ 0.119537] usbcore: registered new interface driver usbfs
[ 0.119842] usbcore: registered new interface driver hub
[ 0.120056] usbcore: registered new device driver usb
[ 0.120178] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.120483] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.121582] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.123443] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.125823] print_constraints: VRTC:
[ 0.127288] print_constraints: VIO: at 1500 mV
[ 0.129577] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.131896] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.132904] print_constraints: VDD3: 5000 mV
[ 0.134307] print_constraints: VDIG1: at 1800 mV
[ 0.135742] print_constraints: VDIG2: at 1800 mV
[ 0.137145] print_constraints: VPLL: at 1800 mV
[ 0.138580] print_constraints: VDAC: at 1800 mV
[ 0.139984] print_constraints: VAUX1: at 1800 mV
[ 0.141418] print_constraints: VAUX2: at 3300 mV
[ 0.142822] print_constraints: VAUX33: at 3300 mV
[ 0.144256] print_constraints: VMMC: at 3300 mV
[ 0.144744] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.145935] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.147094] Switching to clocksource gp timer
[ 0.162414] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.162597] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.162902] MUSB0 controller's USBSS revision = 4ea20800
[ 0.163482] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18
[ 0.163635] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.163909] MUSB1 controller's USBSS revision = 4ea20800
[ 0.164031] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.164123] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.164245] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.164245] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.164276] usb usb1: Product: MUSB HDRC host driver
[ 0.164276] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.164306] usb usb1: SerialNumber: musb-hdrc.1
[ 0.165069] hub 1-0:1.0: USB hub found
[ 0.165100] hub 1-0:1.0: 1 port detected
[ 0.165618] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19
[ 0.166015] NET: Registered protocol family 2
[ 0.166229] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.166503] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.166656] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.166778] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.166778] TCP reno registered
[ 0.166778] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.166809] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.166992] NET: Registered protocol family 1
[ 0.167327] RPC: Registered named UNIX socket transport module.
[ 0.167358] RPC: Registered udp transport module.
[ 0.167358] RPC: Registered tcp transport module.
[ 0.167358] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.167633] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.178894] VFS: Disk quotas dquot_6.5.2
[ 0.178985] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.179504] msgmni has been set to 494
[ 0.182617] alg: No test for stdrng (krng)
[ 0.183288] io scheduler noop registered
[ 0.183288] io scheduler deadline registered
[ 0.183349] io scheduler cfq registered (default)
[ 0.184539] Could not set LED4 to fully on
[ 0.186279] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.805938] console [ttyO0] enabled
[ 0.810211] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.818054] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.825805] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.833618] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.841400] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.858428] brd: module loaded
[ 0.866424] loop: module loaded
[ 0.869934] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.876373] i2c-core: driver [tsl2550] using legacy resume method
[ 0.882812] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.947631] No daughter card found
[ 0.951232] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.966430] Board name: A335X_SK
[ 0.969787] Board version: 1.2B
[ 0.973052] The board is a AM335x Starter Kit.
[ 0.977966] omap_hsmmc.0: alias fck already exists
[ 0.983489] omap_hsmmc.1: alias fck already exists
[ 0.989501] da8xx_lcdc.0: alias fck already exists
[ 0.994964] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel
[ 1.010253] Console: switching to colour frame buffer device 60x34
[ 1.023071] davinci-mcasp.1: alias fck already exists
[ 1.028839] Configure Bluetooth Enable pin...
[ 1.034240] registered am33xx_sr device
[ 1.038513] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator
[ 1.046112] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator
[ 1.074371] lis3lv02d: unknown sensor type 0x87
[ 1.079193] lis3lv02d_i2c: probe of 1-0018 failed with error -22
[ 1.087005] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.094207] omap2-nand driver initializing
[ 1.098663] OneNAND driver initializing
[ 1.103912] CAN device driver interface
[ 1.107971] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.157684] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.164154] davinci_mdio davinci_mdio.0: detected phy mask fffffffc
[ 1.172363] davinci_mdio.0: probed
[ 1.175903] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.183288] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.190979] usbcore: registered new interface driver zd1201
[ 1.196990] usbcore: registered new interface driver cdc_ether
[ 1.203308] usbcore: registered new interface driver cdc_eem
[ 1.209381] usbcore: registered new interface driver dm9601
[ 1.215240] cdc_ncm: 04-Aug-2011
[ 1.218780] usbcore: registered new interface driver cdc_ncm
[ 1.224700] Initializing USB Mass Storage driver...
[ 1.230010] usbcore: registered new interface driver usb-storage
[ 1.236267] USB Mass Storage support registered.
[ 1.241546] mousedev: PS/2 mouse device common for all mice
[ 1.248474] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0
[ 1.256683] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
[ 1.263366] omap_rtc: already running
[ 1.267364] i2c /dev entries driver
[ 1.271423] Linux video capture interface: v2.00
[ 1.276550] usbcore: registered new interface driver uvcvideo
[ 1.282562] USB Video Class driver (1.1.1)
[ 1.288848] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.297332] cpuidle: using governor ladder
[ 1.302124] cpuidle: using governor menu
[ 1.310882] omap4_aes_mod_init: loading AM33X AES driver
[ 1.316528] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.323089] omap4_aes_probe: probe() done
[ 1.327484] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.333648] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.345336] omap4_sham_probe: probe() done
[ 1.352020] usbcore: registered new interface driver usbhid
[ 1.357879] usbhid: USB HID core driver
[ 1.398132] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator
[ 1.405914] _regulator_get: 1-001b supply DVDD not found, using dummy regulator
[ 1.413604] _regulator_get: 1-001b supply AVDD not found, using dummy regulator
[ 1.421264] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator
[ 1.461883] ALSA device list:
[ 1.464996] #0: AM335X EVM
[ 1.468017] oprofile: hardware counters not available
[ 1.473266] oprofile: using timer interrupt.
[ 1.477752] nf_conntrack version 0.5.0 (3957 buckets, 15828 max)
[ 1.484527] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.490203] TCP cubic registered
[ 1.493560] NET: Registered protocol family 17
[ 1.498229] can: controller area network core (rev 20090105 abi 8)
[ 1.504760] NET: Registered protocol family 29
[ 1.509399] can: raw protocol (rev 20090105)
[ 1.513854] can: broadcast manager protocol (rev 20090105 t)
[ 1.519805] Registering the dns_resolver key type
[ 1.524780] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 1.532806] ThumbEE CPU extension supported.
[ 1.537292] mux: Failed to setup hwmod io irq -22
[ 1.542816] Power Management for AM33XX family
[ 1.547668] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.554351] Copied the M3 firmware to UMEM
[ 1.558837] Compensating OPP0 for 0mV Orig nvalue:0x99c3b2 New nvalue:0x99c3b2
[ 1.566436] Compensating OPP1 for 0mV Orig nvalue:0x998e80 New nvalue:0x998e80
[ 1.594451] Compensating OPP0 for 0mV Orig nvalue:0x99bbae New nvalue:0x99bbae
[ 1.602081] Compensating OPP1 for 0mV Orig nvalue:0x999b8c New nvalue:0x999b8c
[ 1.609710] Compensating OPP2 for 0mV Orig nvalue:0xaae6d1 New nvalue:0xaae6d1
[ 1.617340] Compensating OPP3 for 0mV Orig nvalue:0xaacbb8 New nvalue:0xaacbb8
[ 1.625030] create_regulator: VDD1: Failed to create debugfs directory
[ 1.793853] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[ 1.817749] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:54:12 UTC (946688052)
[ 1.826904] Waiting for root device /dev/mmcblk0p2...
[ 1.943237] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.030029] mmc0: new high speed SDHC card at address aaaa
[ 2.037017] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 2.043548] mmcblk0: p1 p2 p3
[ 2.158172] ------------[ cut here ]------------
[ 2.162994] kernel BUG at fs/buffer.c:1265!
[ 2.167358] Internal error: Oops - undefined instruction: 0 [#1]
[ 2.173614] Modules linked in:
[ 2.176788] CPU: 0 Not tainted (3.2.0 #1)
[ 2.181365] PC is at __find_get_block+0x1b4/0x1c4
[ 2.186279] LR is at __getblk+0x28/0x2b8
[ 2.190368] pc : [<c00cec28>] lr : [<c00d13f0>] psr: 20000093
[ 2.190368] sp : cf81dc20 ip : cf81dc68 fp : cf81dc64
[ 2.202331] r10: 00000000 r9 : 00000001 r8 : 00000400
[ 2.207763] r7 : 00000400 r6 : 00000000 r5 : 00000400 r4 : cfbbd380
[ 2.214569] r3 : 00000000 r2 : 00000001 r1 : 00000080 r0 : cf402c80
[ 2.221374] Flags: nzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 2.229064] Control: 10c5387d Table: 80004019 DAC: 00000015
[ 2.235076] Process swapper (pid: 1, stack limit = 0xcf81c2f0)
[ 2.241149] Stack: (0xcf81dc20 to 0xcf81e000)
[ 2.245697] dc20: cf81dc54 cf81dc30 c01d5a98 c01d5858 cf81ddb8 cf81dc8e ffffffff cf81ddd0
[ 2.254211] dc40: cf81ddb8 cfbbd380 00000400 00000000 00000400 00000000 cf81dccc cf81dc68
[ 2.262756] dc60: c00d13f0 c00cea80 00000400 00000000 00000000 00000000 00000001 cf402c80
[ 2.271270] dc80: 00000001 00000002 cf402ac0 cf32dc00 cf81dcbc cf81dca0 cf81dcbc cf81dca8
[ 2.279815] dca0: c00d4dac cfbbd380 cfb6cc00 00000000 00000400 00000000 00000001 00000001
[ 2.288330] dcc0: cf81dcec cf81dcd0 c00d16ec c00d13d4 00000400 cf81dce0 c00d6600 cfbbd380
[ 2.296844] dce0: cf81ddac cf81dcf0 c0111aec c00d16dc 00000400 cf81dd00 c01d7f34 c01d719c
[ 2.305389] dd00: 00000002 0000000a ffffffff ffffffff cf81dd3c c060b900 00000020 cf81ddb0
[ 2.313903] dd20: ff0a0210 ffffffff c060ccec cf81ddb0 00000002 cfb5d800 cfb5d80c cfb6cc00
[ 2.322448] dd40: 00008000 00000000 cf81dd6c 00000001 c01d805c c01d7bdc cf81ddac cf81dd74
[ 2.330963] dd60: cf81dd9c cf81dd78 c00fcd38 c01d8044 c05192c0 00000000 00000000 00000000
[ 2.339477] dd80: 00000400 cf402c80 00000083 cf402ce4 00008000 cfb6cc00 00008000 00000000
[ 2.348022] dda0: cf81ddf4 cf81ddb0 c00ab33c c0111a0c 62636d6d 70306b6c cf810032 cf81ddc8
[ 2.356536] ddc0: c01ccce0 c00a56d0 c0658e68 cf810270 00008000 00000000 cfb6bac0 c060ccd4
[ 2.365081] dde0: 00000000 00000000 cf81de0c cf81ddf8 c010f2e8 c00ab1e8 c0111a00 c008e2dc
[ 2.373596] de00: cf81de44 cf81de10 c00abcb4 c010f2d4 cf81de44 cf81de20 c00c1c50 cf810200
[ 2.382141] de20: c060ccd4 cfb6bac0 00008000 00000000 00008000 00000000 cf81de6c cf81de48
[ 2.390655] de40: c00c1f28 c00abc74 00000000 c060ccd4 cfb6bb40 00000000 cfb6bac0 00008000
[ 2.399169] de60: cf81de94 cf81de70 c00c20ec c00c1ee0 00000000 00008000 00000000 cfb6bac0
[ 2.407714] de80: cfb6bb40 00000020 cf81deec cf81de98 c00c3750 c00c20bc 00000000 00000000
[ 2.416229] dea0: c04ff6c8 00000000 cf81ded4 cf81deb8 c008e234 c008e13c cf810b00 cf40ee98
[ 2.424774] dec0: 00000000 cfb6e000 c04ff6c8 00000000 00008000 c04ff6c8 00000000 00000000
[ 2.433288] dee0: cf81df24 cf81def0 c00c3fa4 c00c35f4 00000000 00000000 00000000 00000000
[ 2.441833] df00: cfb6bac0 cfb6bb40 cf93a000 c05cd1fc cf93a000 00008000 cf81df4c cf81df28
[ 2.450347] df20: c059eaa4 c00c3f24 00000000 cf81df38 0b300002 cf93a000 c05cd1fc cf93a000
[ 2.458862] df40: cf81df9c cf81df50 c059ec2c c059ea80 cf81df8c cf81df60 c00b6308 c00b1edc
[ 2.467407] df60: cf810b00 cf40a198 c0600050 0b300002 c05cd20d c00413ec 0b300002 c05cd20d
[ 2.475921] df80: c00413ec 00000013 00000000 00000000 cf81dfbc cf81dfa0 c059ef1c c059eb3c
[ 2.484466] dfa0: 000000b3 c0644220 c05cd20d c0644220 cf81dfdc cf81dfc0 c059f0bc c059ee50
[ 2.492980] dfc0: cf81dfdc cf81dfd0 c05db440 c05db440 cf81dff4 cf81dfe0 c059e90c c059ef30
[ 2.501525] dfe0: 00000000 c059e7e8 00000000 cf81dff8 c00413ec c059e7f4 ffffffff ffffffff
[ 2.510040] Backtrace:
[ 2.512603] [<c00cea74>] (__find_get_block+0x0/0x1c4) from [<c00d13f0>] (__getblk+0x28/0x2b8)
[ 2.521484] r8:00000000 r7:00000400 r6:00000000 r5:00000400 r4:cfbbd380
[ 2.528472] [<c00d13c8>] (__getblk+0x0/0x2b8) from [<c00d16ec>] (__bread+0x1c/0xdc)
[ 2.536468] [<c00d16d0>] (__bread+0x0/0xdc) from [<c0111aec>] (ext3_fill_super+0xec/0x186c)
[ 2.545166] r4:cfbbd380
[ 2.547821] [<c0111a00>] (ext3_fill_super+0x0/0x186c) from [<c00ab33c>] (mount_bdev+0x160/0x18c)
[ 2.557006] [<c00ab1dc>] (mount_bdev+0x0/0x18c) from [<c010f2e8>] (ext3_mount+0x20/0x28)
[ 2.565460] [<c010f2c8>] (ext3_mount+0x0/0x28) from [<c00abcb4>] (mount_fs+0x4c/0x188)
[ 2.573730] [<c00abc68>] (mount_fs+0x0/0x188) from [<c00c1f28>] (vfs_kern_mount+0x54/0x94)
[ 2.582336] [<c00c1ed4>] (vfs_kern_mount+0x0/0x94) from [<c00c20ec>] (do_kern_mount+0x3c/0xd8)
[ 2.591308] r8:00008000 r7:cfb6bac0 r6:00000000 r5:cfb6bb40 r4:c060ccd4
[ 2.598144] r3:00000000
[ 2.600860] [<c00c20b0>] (do_kern_mount+0x0/0xd8) from [<c00c3750>] (do_mount+0x168/0x6d8)
[ 2.609497] r8:00000020 r7:cfb6bb40 r6:cfb6bac0 r5:00000000 r4:00008000
[ 2.616302] r3:00000000
[ 2.619049] [<c00c35e8>] (do_mount+0x0/0x6d8) from [<c00c3fa4>] (sys_mount+0x8c/0xcc)
[ 2.627227] [<c00c3f18>] (sys_mount+0x0/0xcc) from [<c059eaa4>] (do_mount_root+0x30/0xbc)
[ 2.635742] r7:00008000 r6:cf93a000 r5:c05cd1fc r4:cf93a000
[ 2.641662] [<c059ea74>] (do_mount_root+0x0/0xbc) from [<c059ec2c>] (mount_block_root+0xfc/0x228)
[ 2.650909] r6:cf93a000 r5:c05cd1fc r4:cf93a000
[ 2.655731] [<c059eb30>] (mount_block_root+0x0/0x228) from [<c059ef1c>] (mount_root+0xd8/0xe0)
[ 2.664733] [<c059ee44>] (mount_root+0x0/0xe0) from [<c059f0bc>] (prepare_namespace+0x198/0x1d4)
[ 2.673889] r4:c0644220
[ 2.676513] [<c059ef24>] (prepare_namespace+0x0/0x1d4) from [<c059e90c>] (kernel_init+0x124/0x130)
[ 2.685852] r5:c05db440 r4:c05db440
[ 2.689605] [<c059e7e8>] (kernel_init+0x0/0x130) from [<c00413ec>] (do_exit+0x0/0x67c)
[ 2.697845] r5:c059e7e8 r4:00000000
[ 2.701599] Code: eaffffc1 e1a00004 ebffff6e eaffffdb (e7f001f2)
[ 2.708007] ---[ end trace 4465db959acc9ec9 ]---
[ 2.712921] mmc_wait_for_cmd : cmd->opcode = 52
[ 2.718048] Kernel panic - not syncing: Attempted to kill init!
[ 2.724273] Backtrace:
[ 2.726837] [<c0017978>] (dump_backtrace+0x0/0x110) from [<c0422540>] (dump_stack+0x18/0x1c)
[ 2.735656] r6:c05ffcf4 r5:c05ffcf4 r4:c06451c8 r3:c05fe6c8
[ 2.741577] [<c0422528>] (dump_stack+0x0/0x1c) from [<c04225b0>] (panic+0x6c/0x1a0)
[ 2.749572] [<c0422544>] (panic+0x0/0x1a0) from [<c0041998>] (do_exit+0x5ac/0x67c)
[ 2.757476] r3:cf81bd24 r2:cf81da7c r1:cf81da7c r0:c0510490
[ 2.763397] r7:cf81bc00
[ 2.766052] [<c00413ec>] (do_exit+0x0/0x67c) from [<c0017c68>] (die+0x128/0x2d8)
[ 2.773773] r7:cf81daea
[ 2.776428] [<c0017b40>] (die+0x0/0x2d8) from [<c0017e38>] (arm_notify_die+0x20/0x58)
[ 2.784606] [<c0017e18>] (arm_notify_die+0x0/0x58) from [<c0008350>] (do_undefinstr+0x13c/0x154)
[ 2.793792] [<c0008214>] (do_undefinstr+0x0/0x154) from [<c0013f28>] (__und_svc+0x48/0x60)
[ 2.802398] Exception stack(0xcf81dbd8 to 0xcf81dc20)
[ 2.807678] dbc0: cf402c80 00000080
[ 2.816223] dbe0: 00000001 00000000 cfbbd380 00000400 00000000 00000400 00000400 00000001
[ 2.824737] dc00: 00000000 cf81dc64 cf81dc68 cf81dc20 c00d13f0 c00cec28 20000093 ffffffff
[ 2.833282] r7:00000000 r6:c0014194 r5:20000093 r4:c00cec2c
[ 2.839202] [<c00cea74>] (__find_get_block+0x0/0x1c4) from [<c00d13f0>] (__getblk+0x28/0x2b8)
[ 2.848114] r8:00000000 r7:00000400 r6:00000000 r5:00000400 r4:cfbbd380
[ 2.855133] [<c00d13c8>] (__getblk+0x0/0x2b8) from [<c00d16ec>] (__bread+0x1c/0xdc)
[ 2.863128] [<c00d16d0>] (__bread+0x0/0xdc) from [<c0111aec>] (ext3_fill_super+0xec/0x186c)
[ 2.871826] r4:cfbbd380
[ 2.874481] [<c0111a00>] (ext3_fill_super+0x0/0x186c) from [<c00ab33c>] (mount_bdev+0x160/0x18c)
[ 2.883666] [<c00ab1dc>] (mount_bdev+0x0/0x18c) from [<c010f2e8>] (ext3_mount+0x20/0x28)
[ 2.892120] [<c010f2c8>] (ext3_mount+0x0/0x28) from [<c00abcb4>] (mount_fs+0x4c/0x188)
[ 2.900390] [<c00abc68>] (mount_fs+0x0/0x188) from [<c00c1f28>] (vfs_kern_mount+0x54/0x94)
[ 2.909027] [<c00c1ed4>] (vfs_kern_mount+0x0/0x94) from [<c00c20ec>] (do_kern_mount+0x3c/0xd8)
[ 2.917999] r8:00008000 r7:cfb6bac0 r6:00000000 r5:cfb6bb40 r4:c060ccd4
[ 2.924835] r3:00000000
[ 2.927581] [<c00c20b0>] (do_kern_mount+0x0/0xd8) from [<c00c3750>] (do_mount+0x168/0x6d8)
[ 2.936187] r8:00000020 r7:cfb6bb40 r6:cfb6bac0 r5:00000000 r4:00008000
[ 2.943023] r3:00000000
[ 2.945770] [<c00c35e8>] (do_mount+0x0/0x6d8) from [<c00c3fa4>] (sys_mount+0x8c/0xcc)
[ 2.953948] [<c00c3f18>] (sys_mount+0x0/0xcc) from [<c059eaa4>] (do_mount_root+0x30/0xbc)
[ 2.962493] r7:00008000 r6:cf93a000 r5:c05cd1fc r4:cf93a000
[ 2.968414] [<c059ea74>] (do_mount_root+0x0/0xbc) from [<c059ec2c>] (mount_block_root+0xfc/0x228)
[ 2.977661] r6:cf93a000 r5:c05cd1fc r4:cf93a000
[ 2.982513] [<c059eb30>] (mount_block_root+0x0/0x228) from [<c059ef1c>] (mount_root+0xd8/0xe0)
[ 2.991485] [<c059ee44>] (mount_root+0x0/0xe0) from [<c059f0bc>] (prepare_namespace+0x198/0x1d4)
[ 3.000671] r4:c0644220
[ 3.003326] [<c059ef24>] (prepare_namespace+0x0/0x1d4) from [<c059e90c>] (kernel_init+0x124/0x130)
[ 3.012664] r5:c05db440 r4:c05db440
[ 3.016418] [<c059e7e8>] (kernel_init+0x0/0x130) from [<c00413ec>] (do_exit+0x0/0x67c)
Please suggest ....
Regards,
Ankur