I'm using OMAP5432 EVM. There is only one CSI port. I would like to know if only one camera can be supported by a CSI?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using OMAP5432 EVM. There is only one CSI port. I would like to know if only one camera can be supported by a CSI?
Hi,
There are two CSI ports on OMAP5432 uEVM:
J2 - Single CSI Camera Expansion Connector (30-pin camera connector)
J18- Dual-CSI/Parallel Expansion Connector (60 pin camera connector)
You can use either J2 or J18. J2 provides single CSI-2 interface, while J18 can be used to provide either dual CSI-2 camera interfaces or a single parallel camera interface.
Best Regards,
Yordan