Other Parts Discussed in Thread: AM1808
I am trying to interface O/P of the demodulator chip to the McBSP interface. My question here is with regard to Frame sync signal. Is it possible to interface only the clock signal and the Serial Data signal to interface to McBSP and ignore the frame sync signal
Since the kind of Frame sync the MCBSP is expecting cannot be generated from the demodulator chip.
The kind of Control signal which comes out of Demod chip is either valid signal which is high for around 190 serial bytes of data or one pulse signal which comes at the begining of data for one clock signal
The ARM Chipset which is being referred here is AM1808. Does AM1808 supports any 656/601 based interface support apart from the uPP interface it has