This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using ezDSP5535 standalone without USB sampling and fft

Hello,

I started with the c55_caf_02.00.02.04 (csl_usb_iso_fullspeed_example) and added a simple frequency/amplitude detector in csl_i2c_power_monitor.c after the FFT in the spectrum display section. It works as expected and now I want to strip it down to run standalone without USB, sampling the input all the time from power on. Is it possible or is there an example better suited to start with for my application that skips the USB part?


Thanks in advance

Tobias