This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

no prints from early printk



Hi All,

 On AM335x EVM, I'm not getting prints from early printk,

My linux .config file says,

CONFIG_DEBUG_LL=y
CONFIG_DEBUG_OMAP2UART1=y
CONFIG_EARLY_PRINTK=y.

1. interpreting CONFIG_DEBUG_OMAP2UART1 as UART1, i also connected to UART1 and checked.No prints found.

2. I enabled CONFIG_SERIAL_2 in uboot but could not transfer uboot.img over uart.

3. I want to see prints from early_printk's  on EVM.

Idea is  to finally use early_printk() enabled kernel on my custom board as I'm not getting any prints from kernel on my custom board.

Regards,

Gangadhar