This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517 G20/G21 pin connection

I made a PCB based on schematics of LogicPD development board TMDSEVM3517. There G20/G21 pins are not connected NC. But in datasheet on ti.com these pins must be connected to GND.
What will be if G20/G21 pins will not be connected to GND?

On my PCB I have some troubles.
GPIO pins 40,39, 42, 41, 108, 107, 112, 114 is not working - after switch pad'а into GPIO mode voltage on PIN was set to 0 and will not changing after writing in GPIO registers.
May it will be affect from not connected pins.