Hi,
I have a question about subFrameMode.
I used the rdk4.0 on DM816x, and I want to realize the image rotation by used tiler, my image resolution is 2952*1936.
I used the link as follow:
capture ->dei0 ->dei1->framesout->...
I enable tiler on dei0, and translate the tiler address to 90-degree address on the output of dei0, and the dei worked on bypass mode.
However, the dei only support the max resolution of image is 1920*1080.
Could I enable the dei subFrameMode to realize the 2592*1936 non-tiler memory to 2592*1936 tilered memory by the deiLink.
Regards,
Tianxing