This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BCP simulation on ccs

hi,

We are testing the BCP hardware accelerator with the test code given for LTE downlink with MCSDK. We are using CCSv5 in simulator mode (6618 functional simulator).  There seems to be issues with BCP process completion interrupt and the code is running infinitely. Console window is pasted below.  BCP works on in emulator mode ?

regards and thanks,

Aswathy

[TMS320C66x_0] **************************************************
*************** BCP Example Start ****************
**************************************************
Using BCP Driver version: 0x1000009 Version Info: BCP Driver Revision: 01.00.00.09:May 13 2014:18:11:11
[Core 0]: L1D cache size 0. L2 cache size 0.
ipc started
SRIO powered on
[Core 0]: BCP instance 0 successfully initialized
System init done
Tasks scheduled and BIOS begins
[Core 0]: BCP driver successfully opened
Global FDQ 897 successfully setup with 256 descriptors


-------------- LTE DL Test Start --------------
Rx FDQ 736 successfully setup with 62 descriptors
Flow 0 opened to send data to RxQ: 900
Tx FDQ 737 successfully setup with 2 descriptors
Reading test configuration ...
Waiting on output from BCP ...