This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Keystone Link State Monitoring

Hi,

I have a 6638 EVM. I've checked GbE SW phy alive status and link status registers. For port 2 they're fine. For port 1 phy is not alive however i can send and receive frames via port 1. Is behaviour  of port 1 normal? 

Thanks,

Burhan. 

  • Burhan,

    If you are using XTCIEVMK2X, please find the below information, and also clearly mention the name of device and board using by you.
    XTCIEVMK2X:
    Here, the Ethernet PHY (PHY1 and PHY2) is connected to SoC EMAC0 & 1 to provide a copper interface and routed to a Gigabit RJ-45 connector (LAN1). If you have the board revison is 1.0/1.1, see the known issue document(EVMK2HX_Rev1_1_Known_Issues) available at advantech page.

  • Sorry for consuming your time, I was giving wrong Phy Addresses. 

    Burhan.