This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x - Kernel 3.12.20 MUSB Problem

Hi,

I'm building a kernel from source (Arago-Dora) based on SDK 7.0.

I've having issues getting the MUSB driver to enumerate on boot.  I've applied one of the patches suggested to move the DMA controller to the top in am33xx.dtsi. 

http://www.spinics.net/lists/linux-omap/msg105854.html

I've tried building MUSB_HDRC into the kernel as well as making it a module without any luck.

I've compared the am335x-evmsdk.dts, am335x-evm.dts and am33xx.dtsi against those found in SDK 7.0 and fixed a couple minor issues with the ctrl-mod address (@441e000).

Comparing this build to a working SDK 6.0 build, I never see the cppi41dma registration messages or the musb driver messages on boot.

Any ideas?

Thanks,

Robert