This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resume from Standby - Falls back to sleep

Hi All,


I am running Android 4.1.2 on AM335x, issuing a sleep command with echo mem > /sys/power/state.


I attempt to wake from standby with GPIO button - I see on the console that the system starts to wake up, but then falls back to sleep every time.


I found that I can successfully resume the system if I hold the touch screen while I press the button. Could the issue be that the system isn't grabbing a wakelock in time? Has anyone experienced something like this?

Many Thanks! Here is a console log of a resume attempt:

[  270.197113] GFX domain entered low power state                                            
[  270.202056] Successfully transitioned all domains to low power state                      
[  270.417388] PM: early resume of devices complete after 208.059 msecs                      
[  270.487915] android_work: sent uevent USB_STATE=DISCONNECTED                              
[  270.557525] android_work: sent uevent USB_STATE=CONNECTED                                 
[  270.563385] android_work: sent uevent USB_STATE=DISCONNECTED                              
[  270.649291] android_work: sent uevent USB_STATE=CONNECTED                                 
[  270.656066]  gadget: high-speed config #1: android                                        
[  270.661285] android_work: sent uevent USB_STATE=CONFIGURED                                                       
[  270.699035] wakeup wake lock: event0-272                                                  
[  270.705413] wl12xx: state: 0                                                              
[  271.165985] wl12xx: firmware booted (Rev 6.3.10.0.132)                                    
[  271.183807] wl12xx: state: 2                                                              
[  271.187347] wl12xx: adding p2p mgmt vif                                                   
[  271.219116] PM: resume of devices complete after 794.273 msecs                                                                    
[  271.236389] Restarting tasks ...                                                          
[  271.256835] adb_release                                                                   
[  271.302825] adb_open                                                                      
[  271.327972] done.                                                                                                                             
[  271.393768] suspend: exit suspend, ret = 0 (2000-01-01 00:04:28.690028522 UTC)            
[  271.417449] active wake lock PowerManagerService                                          
[  271.422302] active wake lock rx_wake, time left 95                                        

-- Starts to fall asleep here again?

                                                    
[  272.634765] PM: Syncing filesystems ... done.                                                                                                           
[  272.720733] Freezing user space processes ... (elapsed 0.01 seconds) done.                
[  272.740386] Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.                                                            
[  272.788787] wl12xx: down                                                                  
[  272.792205] wl12xx: down                                                                                                                        
[  272.809478] PM: suspend of devices complete after 22.032 msecs                                                                              
[  272.824249] PM: late suspend of devices complete after 1.434 msecs