This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

We met errors using PCI boot on DM6437

We met the following error message while booting by PCI on DM6437.

We met thr following error message on CCS 3.3 using Single Step feature.

We read the data of Main Processor memory area (Freescale Processor) using PCI BUS  

And these error message happen under the condition nearly  "0" degree in case temprature.

(error messages)

Can't Single Step Target Program:

Error 0x00000020/-1202

Error during: Execution,

 

CPU pipeline is stalled and the CPU is 'not ready'. This means

that the CPU has performed an access which has not

completed, and the CPU is waiting. The target may need to be

reset. The user can choose 'Yes' to force the CPU to be 'ready'.

When this is done, the user will have the ability to examine

the target memory and registers to determine the cause of the

CPU stall. If CPU hang is caused by application and it has been

forced to be 'ready', the CPU should not be run without a reset.

 Yes    - - force CPU ready (might corrupt the code)

 Disconnect  - disconnect CCS so that it can be reset

Retry - attempt the command again.

 

Sequence ID: 14

Error Code: -1202

Error Class: 0x00000020

 

After the above error message, we met the following error messaga, when we read DDR2 content.

(error messages)

Trouble Reading Memory Block at 0x80000000 on Page 0 of Length 0x30:

Error 0x00000002/-1202

Error during: Memory,

CPU pipeline is stalled and the CPU is 'not ready'. This means

that the CPU has performed an access which has not

completed, and the CPU is waiting. The target may need to be

reset. The user can choose 'Yes' to force the CPU to be 'ready'.

When this is done, the user will have the ability to examine

the target memory and registers to determine the cause of the

CPU stall. If CPU hang is caused by application and it has been

forced to be 'ready', the CPU should not be run without a reset.

Yes    - force CPU ready (might corrupt the code)

Disconnect - disconnect CCS so that it can be reset

Retry - attempt the command again

 

(My question)

When we met the above error message, does it show DM6437's core exceed 100% of the its perofomance?

Whta is the reason the following message happen?

To avoid the following error message, what issues we shoukd reconsider ?