Hello,
I use dualserver software as DHCP server in WINXP
My computer has two network cards 100M and 1000M
I use the TI AM335X Starter kt (SDK 6.0) to test udhcpc
when i use 100M network card to test AM335X udhcpc, it is ok to get IP
but if i use the 1000M network card, it is fail to get IP ,and udhcpc is keeping to show Sending discover...
Someone knows why???
P/S:
If i use the 1000M network card and setting static IP to test TCP Communications,it is OK!!