Hi ,
I am working AM335x Rev 1.1A EVM board and software i am using ti-sdk-am335x-evm-07.00.00.00. Now I want to run standalone helloworld application on this board (at U-boot). I am able to load the application successfully but while executing it and getting data abort.
U-Boot# tftpboot 0x80200000 /tftpboot/hello_world.bin
U-Boot# go 0x80200000 Hello World ? This is test !!!
## Starting application at 0x80200000 ...
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<802000ec>] lr : [<80200024>]
sp : 9f32ae00 ip : 0000000f fp : 9f32db68
r10: 9f7a5324 r9 : 9f32af38 r8 : 00000009
r7 : 9f32dc48 r6 : 9f32dc4c r5 : 00000008 r4 : 00000000
r3 : 80208254 r2 : 80208254 r1 : 00000006 r0 : 802001cf
Flags: nZCv IRQs on FIQs on Mode SVC_32
Resetting CPU ...
resetting ...
Help on this issue..
Regards,
Bhimesh