Hi,
I am using the 6657 DSP.
I want to build an application for sending an image over the PCIe to the DSP.
Before the DSP boots, I need to perform a checksum on the received image.If checksum OK, Boot the DSP with the image and turn on GPIO leds.
1. How Can I download a custom RBL (boot loader) to the DSP ? at which address does it start, at address of 0x20B00000 ?
2. How can I check checksum on an image (*.bin) file ? Is the checksum value exist in the file ?
Thanks,
Ivgeni.