I want to develop a DVR with DM8165, here is several questions about the compositor/HDVPSS/HDVICP2 I want to confirm: 1. I want to display 2*1080P videos (from Vin0 and Vin1) in one screen at the same time, can the DM8165 support it? If can, how many videos can the DM8165 support to composite in one stream (I want to composite 5 videos to one stream)? 2. The HDVPSS of DM8165 can support two 1080P videos input in 60FPS each port, can I get the 4*1080P videos input but only in 25-30FPS each port? If can, how to do? 3. Can the DM8165 support 2*1080P (30FPS) encode and 1*VGA (30FPS) encode at the same time?Thanks.