Other Parts Discussed in Thread: AM3517
Team,
We are trying to do some benchmarks with the LogicPD AM3517 eXperimenter's board. We are trying to find a quick and dirty example that will toggle a GPIO pin without using an OS - we need something like StarterWare that can be loaded in via an emulator. Basically, set a bit, run a bunch of different benchmarks, and then clear it so we can measure the time needed to run the code.
Is there something like this that we can use, or will we need to figure it out from the ground up? It would seem like a very common use case, just for bringing a board up to see if it works.
Thanks,
John