There are three conditions to set AM3352 RTC features.
1. RTC-only mode
2. Using RTC feature but without RTC-only mode support
3. RTC features disable
Does it mean AM3352 internal RTC LDO is actived for souring on chip 32.768KHz and can use it for RTC-only
power saving mode and all RTC functions at condition 1?
At condition 3, internal RTC LDO logic is disabled totally and on chip 32.768KHz lose its function.
RTC function is totally disabled.
At condition 2, internal RTC LDO logic is disabled partially and on chip 32.768KHz lose its function,also.
If we want to use RTC function,we should add an external 32.768KHz for supporting this features.
right?