Other Parts Discussed in Thread: DM3730, WL1271, SYSCONFIG, ADS7846, OMAP3530, DAC7512, TCA6416, TSC2007, TSC2004, PCF8574, LM63, LM70, LM73, LM77, LM80, LM83, LM87, LM90, LM92, LM93, LM95241, ADS7828, ADS7871, AMC6821, TMP102, TMP401, TMP421, TPS65010, TWL6030, BQ24022, LP3971, LP3972, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS7303, DA8XX
Hi,
I need to solve this issue which I have got at the moment. I am booting Linux Kernel from SD card the issue I am facing is that the SD card boot works OK on the dev kit from varascite but does not work with custom hardware. What I get is unable to mount rootfs even though the kernel image is read from the SD card and not on NAND. The only boot loader I have on NAND are MLO and u-boot
What I have noticed is the my SD card comes up as ro and not sure what the problem here could be. The other thing I have is that the PIN_MUX for MMC1 on DM3730 were using PULL UP Enabled with no external pull ups. What I have done is disabled the internal pull ups as the board has external pull ups on MMC1_CMD, MMC1_DAT0, MMC1_DAT1, MMC1_DAT2 and MMC1_DAT3.
I am not sure what else I can do. I did format the card few times and installed the file system manually but to no avail. I have also tried changing the card but nothing seems to get me going in terms of mounting the filesystem. Any help would be great.
My Environmental variables are
setenv ethaddr 00:11:22:33:44:55
setenv ipaddr 1.1.1.1
setenv serverip 1.1.1.11
setenv netmask 255.255.255.0
setenv gatewayip 192.168.1.1
setenv bootdelay 1
setenv console_tty ttyO2
setenv get_kernel run nand_kernel
setenv nand_kernel nand read.i 0x80000000 280000 300000
setenv mmc_kernel 'mmc init; fatload mmc 1 0x80000000 uImage'
setenv tftp_kernel tftpboot 0x80000000 uImage
set addmac setenv bootargs \${bootargs} ethaddr=\${ethaddr}
set addconsole setenv bootargs \${bootargs} console=\${console_tty},115200n8 androidboot.console=\${console_tty}
setenv bootargs_common init=/init mem=256M noinitrd rw omap_vout.vid1_static_vrfb_alloc=y vram=8M omapfb.vram=0:8M rootdelay=1 rootwait
setenv setargs_fs set bootargs \${bootargs_common} root=/dev/mtdblock4 rootfstype=jffs2 ip=::::::off
setenv setargs_nfs set bootargs \${bootargs_common} root=/dev/nfs nfsroot=\${nfsroot},nolock ip=dhcp
setenv setargs_sd set bootargs \${bootargs_common} root=/dev/mmcblk0p2 ip=off
setenv boot_fs run get_kernel\;run setargs_fs\;run addmac\;run addconsole\;bootm 0x80000000
setenv boot_nfs run tftp_kernel\;run setargs_nfs\;run addmac\;run addconsole\;bootm 0x80000000
setenv boot_sd run mmc_kernel\;run setargs_sd\;run addmac\;run addconsole\;bootm 0x80000000
setenv bootcmd run boot_sd
saveenv
-----------------------------------------------------------------------------------------------------------------------------------------------------------
LOGS
Texas Instruments X-Loader 1.51 (Jul 1 2014 - 04:10:33)
Booting from nand . . .
Starting OS Bootloader...
U-Boot 2010.06 (Jul 01 2014 - 04:11:20)
OMAP34xx/35xx-GP ES2.1, CPU-OPP2 L3-165MHz
VAR-SOM-OM3xxx Board + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: 512 MiB
In: serial
Out: serial
Err: serial
Net: smc911x-0
Hit any key to stop autoboot: 1 0
mmc1 is available
reading uImage
3029708 bytes read
## Booting kernel from Legacy Image at 80000000 ...
Image Name: Linux-2.6.37-00002-g52e1f5d
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3029644 Bytes = 2.9 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
[ 0.000000] Linux version 2.6.37-00002-g52e1f5d (ali@ubuntu) (gcc version 4.4.3 (GCC) ) #2 Tue Jul 1 05:28:42 PDT 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: VARISCITE VAR-SOM-OM3X
[ 0.000000] Reserving 8388608 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] OMAP3630 ES1.2 (l2cache iva sgx neon isp 192mhz_clk )
[ 0.000000] SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x10000
[ 0.000000] On node 0 totalpages: 63488
[ 0.000000] free_area_init_node: node 0, pgdat c05fb0b0, node_mem_map c06cf000
[ 0.000000] Normal zone: 512 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 62976 pages, LIFO batch:15
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 62976
[ 0.000000] Kernel command line: init=/init mem=256M noinitrd rw omap_vout.vid1_static_vrfb_alloc=y vram=8M omapfb.vram=0:8M rootdelay=1 rootwait root=/dev/mmcblk0p2 ip=off ethaddr=00:11:22:33:44:55 console=ttyO2,115200n8 androidboot.console=ttyO2
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 248MB = 248MB total
[ 0.000000] Memory: 244692k/244692k available, 17452k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc003f000 ( 220 kB)
[ 0.000000] .text : 0xc003f000 - 0xc05b8000 (5604 kB)
[ 0.000000] .data : 0xc05b8000 - 0xc060a2c0 ( 329 kB)
[ 0.000000] NR_IRQS:409
[ 0.000000] Clocking rate (Crystal/Core/MPU): 26.0/400/800 MHz
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
[ 0.000000] Total of 96 interrupts on 1 active controller
[ 0.000000] GPMC revision 5.0
[ 0.000000] Trying to install interrupt handler for IRQ402
[ 0.000000] Trying to install interrupt handler for IRQ403
[ 0.000000] Trying to install interrupt handler for IRQ404
[ 0.000000] Trying to install interrupt handler for IRQ405
[ 0.000000] Trying to install interrupt handler for IRQ406
[ 0.000000] Trying to install interrupt handler for IRQ407
[ 0.000000] Trying to install interrupt handler for IRQ408
[ 0.000000] Trying to install type control for IRQ409
[ 0.000000] Trying to set irq flags for IRQ409
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] Console: colour dummy device 80x30
[ 0.000000] Calibrating delay loop... 799.29 BogoMIPS (lpj=3121152)
[ 0.000000] pid_max: default: 32768 minimum: 301
[ 0.000000] Security Framework initialized
[ 0.000000] Mount-cache hash table entries: 512
[ 0.000000] CPU: Testing write buffer coherency: ok
[ 0.000000] regulator: core version 0.5
[ 0.000000] regulator: dummy:
[ 0.000000] NET: Registered protocol family 16
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] OMAP GPIO hardware version 2.5
[ 0.000000] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.000000] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.000000] OMAP DMA hardware revision 5.0
[ 0.022369] bio: create slab <bio-0> at 0
[ 0.026397] regulator: vwl1271: 1800 mV
[ 0.030487] SCSI subsystem initialized
[ 0.037384] usbcore: registered new interface driver usbfs
[ 0.042083] usbcore: registered new interface driver hub
[ 0.046417] usbcore: registered new device driver usb
[ 0.051879] omap_i2c omap_i2c.1: bus 1 rev4.0 at 2600 kHz
[ 0.059020] twl4030: PIH (irq 7) chaining IRQs 368..375
[ 0.063720] twl4030: power (irq 373) chaining IRQs 376..383
[ 0.068756] twl4030: gpio (irq 368) chaining IRQs 384..401
[ 0.075592] regulator: VUSB1V5: 1500 mV normal standby
[ 0.080383] regulator: VUSB1V8: 1800 mV normal standby
[ 0.085113] regulator: VUSB3V1: 3100 mV normal standby
[ 0.091857] twl4030_usb twl4030_usb: Initialized TWL4030 USB module
[ 0.097839] regulator: VIO: 1800 mV normal standby
[ 0.104370] regulator: VMMC1: 1850 <--> 3150 mV at 3000 mV normal standby
[ 0.108886] regulator: VDAC: 1800 mV normal standby
[ 0.113922] regulator: VAUX2_4030: 2800 mV normal standby
[ 0.118560] regulator: VPLL2: 1800 mV normal standby
[ 0.124938] regulator: VSIM: 1800 <--> 3000 mV at 1800 mV normal standby
[ 0.129547] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.134277] omap_i2c omap_i2c.3: bus 3 rev4.0 at 400 kHz
[ 0.141052] Advanced Linux Sound Architecture Driver Version 1.0.23.
[ 0.144317] Bluetooth: Core ver 2.15
[ 0.148010] NET: Registered protocol family 31
[ 0.153442] Bluetooth: HCI device and connection manager initialized
[ 0.157409] Bluetooth: HCI socket layer initialized
[ 0.161468] Switching to clocksource 32k_counter
[ 0.286346] WL1271: BT_EN GPIO initialized
[ 0.291839] musb-hdrc: version 6.0, otg (peripheral+host), debug=0
[ 0.296417] musb-hdrc musb-hdrc.0: dma type: dma-inventra
[ 0.304779] HS USB OTG: revision 0x40, sysconfig 0x2001, sysstatus 0x1, intrfsel 0x1, simenable 0x0
[ 0.314575] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 0.318176] musb-hdrc: MHDRC RTL version 1.800
[ 0.321136] musb-hdrc: setup fifo_mode 4
[ 0.325439] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 0.332824] musb-hdrc musb-hdrc.0: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
[ 0.336456] Registered /proc/driver/musb_hdrc.0
[ 0.340332] NET: Registered protocol family 2
[ 0.346466] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.353027] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.358734] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.364257] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.366424] TCP reno registered
[ 0.371368] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.376739] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.380279] NET: Registered protocol family 1
[ 0.386138] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.390960] omap-iommu omap-iommu.0: isp registered
[ 0.501647] ashmem: initialized
[ 0.504974] VFS: Disk quotas dquot_6.5.2
[ 0.510406] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.516906] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.520141] msgmni has been set to 477
[ 0.524108] io scheduler noop registered
[ 0.527435] io scheduler deadline registered
[ 0.531280] io scheduler cfq registered (default)
[ 0.593414] OMAP DSS rev 2.0
[ 0.595520] OMAP DISPC rev 3.0
[ 0.597320] OMAP VENC rev 2
[ 0.599487] OMAP DSI rev 1.0
[ 0.933258] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.941009] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 72) is a OMAP UART0
[ 0.945770] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 73) is a OMAP UART1
[ 0.950469] omap_uart.2: ttyO2 at MMIO 0x49020000 (irq = 74) is a OMAP UART2
[ 1.687805] console [ttyO2] enabled
[ 1.696105] omap_uart.3: ttyO3 at MMIO 0x49042000 (irq = 80) is a OMAP UART3
[ 1.714233] brd: module loaded
[ 1.723358] loop: module loaded
[ 1.732849] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.741851] omap2-nand driver initializing
[ 1.750549] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron )
[ 1.760620] Creating 5 MTD partitions on "omap2-nand.0":
[ 1.769500] 0x000000000000-0x000000080000 : "X-Loader-NAND"
[ 1.780212] 0x000000080000-0x0000001c0000 : "U-Boot-NAND"
[ 1.791259] 0x0000001c0000-0x000000280000 : "Boot Env-NAND"
[ 1.801849] 0x000000280000-0x000000780000 : "Kernel-NAND"
[ 1.814483] 0x000000780000-0x000020000000 : "File System - NAND"
[ 2.032318] OneNAND driver initializing
[ 2.040344] smsc911x: Driver version 2008-10-21.
[ 2.048248] smsc911x-mdio: probed
[ 2.057128] eth0: attached PHY driver [SMSC LAN8700] (mii_bus:phy_addr=ffffffff:01, irq=-1)
[ 2.069488] smsc911x: get mac from cmd line.
[ 2.077453] ethaddr parsed from commandline: 00:11:22:33:44:55
[ 2.086425] net eth0: MAC Address: 00:11:22:33:44:55
[ 2.095153] usbcore: registered new interface driver asix
[ 2.104461] usbcore: registered new interface driver cdc_ether
[ 2.114074] usbcore: registered new interface driver net1080
[ 2.123687] usbcore: registered new interface driver cdc_subset
[ 2.133331] usbcore: registered new interface driver zaurus
[ 2.142608] usbcore: registered new interface driver zd1201
[ 2.152435] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.163330] ehci-omap.0 supply hsusb0 not found, using dummy regulator
[ 3.180572] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 3.191192] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 3.202423] ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
[ 3.227600] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 3.237884] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.249511] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.260162] usb usb1: Product: OMAP-EHCI Host Controller
[ 3.269836] usb usb1: Manufacturer: Linux 2.6.37-00002-g52e1f5d ehci_hcd
[ 3.279388] usb usb1: SerialNumber: ehci-omap.0
[ 3.286926] hub 1-0:1.0: USB hub found
[ 3.293060] hub 1-0:1.0: 3 ports detected
[ 3.328704] Initializing USB Mass Storage driver...
[ 3.337646] usbcore: registered new interface driver usb-storage
[ 3.346557] USB Mass Storage support registered.
[ 3.352478] android init
[ 3.357330] android_probe pdata: c05c8700
[ 3.362792] android_bind
[ 3.367004] android_bind_config
[ 3.373504] android_usb gadget: android_usb ready
[ 3.381530] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 3.391754] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 3.403839] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 3.415435] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.425872] usb usb2: Product: MUSB HDRC host driver
[ 3.435180] usb usb2: Manufacturer: Linux 2.6.37-00002-g52e1f5d musb-hcd
[ 3.444732] usb usb2: SerialNumber: musb-hdrc.0
[ 3.452209] hub 2-0:1.0: USB hub found
[ 3.458251] hub 2-0:1.0: 1 port detected
[ 3.463989] f_adb init
[ 3.468627] android_register_function adb
[ 3.474334] f_mass_storage init
[ 3.480590] fsg_probe pdev: c05c8310, pdata: c05c8734
[ 3.489044] android_register_function usb_mass_storage
[ 3.495697] adb_bind_config
[ 3.503845] android_usb gadget: Mass Storage Function, version: 2009/09/11
[ 3.513671] android_usb gadget: Number of LUNs=1
[ 3.521301] lun0: LUN: removable file: (no medium)
[ 3.530151] mice: PS/2 mouse device common for all mice
[ 3.539794] ads7846 spi1.0: touchscreen, irq 337
[ 3.550689] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input0
[ 3.568145] input: twl4030_pwrbutton as /devices/platform/omap/omap_i2c.1/i2c-1/1-0049/twl4030_pwrbutton/input/input1
[ 3.583618] using rtc device, twl_rtc, for alarms
[ 3.592102] twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
[ 3.602508] i2c /dev entries driver
[ 3.609466] Linux media interface: v0.10
[ 3.616333] Linux video capture interface: v2.00
[ 3.625762] OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
[ 3.636535] usb 1-1: new high speed USB device using ehci-omap and address 2
[ 3.646942] device-mapper: uevent: version 1.0.3
[ 3.657684] device-mapper: ioctl: 4.18.0-ioctl (2010-06-29) initialised: dm-devel@redhat.com
[ 3.669067] Bluetooth: HCI UART driver ver 2.2
[ 3.676452] Bluetooth: HCI H4 protocol initialized
[ 3.684143] Bluetooth: HCILL protocol initialized
[ 3.691375] cpuidle: using governor ladder
[ 3.697753] cpuidle: using governor menu
[ 3.708587] mmci-omap-hs.1 supply vmmc_aux not found, using dummy regulator
[ 3.721282] usbcore: registered new interface driver usbhid
[ 3.729187] usbhid: USB HID core driver
[ 3.736358] logger: created 64K log 'log_main'
[ 3.743927] logger: created 256K log 'log_events'
[ 3.751617] logger: created 64K log 'log_radio'
[ 3.759338] logger: created 64K log 'log_system'
[ 3.768920] usbcore: registered new interface driver snd-usb-audio
[ 3.777923] OMAP3 EVM SoC init
[ 3.811737] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[ 3.823211] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.835693] hub 1-1:1.0: USB hub found
[ 3.843872] hub 1-1:1.0: 4 ports detected
[ 3.859893] asoc: twl4030-hifi <-> omap-mcbsp-dai.1 mapping ok
[ 3.868896] ALSA device list:
[ 3.873199] #0: omap3evm
[ 3.878967] oprofile: hardware counters not available
[ 3.886596] oprofile: using timer interrupt.
[ 3.894805] nf_conntrack version 0.5.0 (3823 buckets, 15292 max)
[ 3.904571] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.911834] TCP cubic registered
[ 3.917572] Initializing XFRM netlink socket
[ 3.924530] NET: Registered protocol family 17
[ 3.931701] NET: Registered protocol family 15
[ 3.938385] Bluetooth: L2CAP ver 2.15
[ 3.945129] Bluetooth: L2CAP socket layer initialized
[ 3.952972] Bluetooth: SCO (Voice Link) ver 0.6
[ 3.960540] Bluetooth: SCO socket layer initialized
[ 3.968597] Bluetooth: RFCOMM TTY layer initialized
[ 3.976684] Bluetooth: RFCOMM socket layer initialized
[ 3.984039] Bluetooth: RFCOMM ver 1.11
[ 3.991058] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.999664] Bluetooth: BNEP filters: protocol multicast
[ 4.008697] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 4.017913] Registering the dns_resolver key type
[ 4.024261] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 4.038452] ThumbEE CPU extension supported.
[ 4.047882] Power Management for TI OMAP3.
[ 4.060821] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 4.073913] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 4.085510] SmartReflex Class3 initialized
[ 4.099090] platform iva.0: omap_voltage_scale: Already at the requestedrate 800000000
[ 4.112487] platform mpu.0: omap_voltage_scale: Already at the requestedrate 1000000000
[ 4.209625] mmc0: new high speed SDHC card at address e624
[ 4.218536] mmcblk0: mmc0:e624 SU04G 3.69 GiB (ro)
[ 4.228942] usb 1-1.1: new high speed USB device using ehci-omap and address 3
[ 4.238403] VAR_SOM_OM3X_enable_lcd
[ 4.243713] mmcblk0: p1 p2 p3
[ 4.325653] twl_rtc twl_rtc: setting system clock to 2000-01-01 00:01:17 UTC (946684877)
[ 4.337310] omap_vout omap_vout: Buffer Size = 3686400
[ 4.360504] omap_vout omap_vout: : registered and initialized video device 0
[ 4.370910] omap_vout omap_vout: Buffer Size = 3686400
[ 4.381652] omap_vout omap_vout: : registered and initialized video device 1
[ 4.392761] Waiting 1sec before mounting root device...
[ 4.432128] usb 1-1.1: New USB device found, idVendor=0424, idProduct=2660
[ 4.443908] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 4.454589] hub 1-1.1:1.0: USB hub found
[ 4.461212] hub 1-1.1:1.0: 3 ports detected
[ 4.760253] usb 1-1.1.1: new high speed USB device using ehci-omap and address 4
[ 4.891357] usb 1-1.1.1: New USB device found, idVendor=0424, idProduct=4040
[ 4.903411] usb 1-1.1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 4.914428] usb 1-1.1.1: Product: Ultra Fast Media Reader
[ 4.922515] usb 1-1.1.1: Manufacturer: Generic
[ 4.929962] usb 1-1.1.1: SerialNumber: 000008264001
[ 4.938568] scsi0 : usb-storage 1-1.1.1:1.0
[ 5.408294] VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
[ 5.420806] Please append a correct "root=" boot option; here are the available partitions:
[ 5.431518] 1f00 512 mtdblock0 (driver?)
[ 5.439514] 1f01 1280 mtdblock1 (driver?)
[ 5.447540] 1f02 768 mtdblock2 (driver?)
[ 5.455535] 1f03 5120 mtdblock3 (driver?)
[ 5.463562] 1f04 516608 mtdblock4 (driver?)
[ 5.471435] b300 3872256 mmcblk0 driver: mmcblk
[ 5.483154] b301 72261 mmcblk0p1 00000000-0000-0000-0000-000000000000mmcblk0p1
[ 5.496856] b302 1935832 mmcblk0p2 00000000-0000-0000-0000-000000000000mmcblk0p2
[ 5.510559] b303 1863540 mmcblk0p3 00000000-0000-0000-0000-000000000000mmcblk0p3
[ 5.524719] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
[ 5.534240] Backtrace:
[ 5.542144] [<c004ee1c>] (dump_backtrace+0x0/0x110) from [<c04482d4>] (dump_stack+0x18/0x1c)
[ 5.551727] r7:c003369c r6:00008000 r5:c060b428 r4:c060b428
[ 5.564697] [<c04482bc>] (dump_stack+0x0/0x1c) from [<c044833c>] (panic+0x64/0x180)
[ 5.577972] [<c04482d8>] (panic+0x0/0x180) from [<c0009214>] (mount_block_root+0x260/0x2b0)
[ 5.587463] r3:00000000 r2:00000000 r1:cf01bf58 r0:c0527c3c
[ 5.601104] [<c0008fb4>] (mount_block_root+0x0/0x2b0) from [<c00092b8>] (mount_root+0x54/0x68)
[ 5.615570] [<c0009264>] (mount_root+0x0/0x68) from [<c0009438>] (prepare_namespace+0x16c/0x1c4)
[ 5.625518] r5:c00336b1 r4:c060a324
[ 5.635681] [<c00092cc>] (prepare_namespace+0x0/0x1c4) from [<c000877c>] (kernel_init+0x114/0x154)
[ 5.645812] r5:c0032c74 r4:c060a2c0
[ 5.655273] [<c0008668>] (kernel_init+0x0/0x154) from [<c007dd48>] (do_exit+0x0/0x638)
[ 5.664428] r5:c0008668 r4:00000000