Hi,
When I am sending an image to the DSP via PCIe.
- Is the existing Boot loader in the EVM checks checksum?
- How Can I download a custom RBL (boot loader) to the DSP and replace the existing one?
- To which BAR the linux machine sends the IMAGE ?
- Where is written the configuration of the mapping between the BARS and address on the DSP ? where is the mapping between DSP address space and the BARS ?
- When the image is copied to L2 core 0 memory space, does the boot loader copies it to another place or runs it from the L2 core 0 memory space ?
- When sending commands from PC to PCIe, to which BAR should I send the commands ?
Thanks,
Ivgeni.