Other Parts Discussed in Thread: 4430
Hi All,
I have compiled the android JB to the panda-board 4430. Since I don't have the CSI camera module too interface it to the panda-board 4430, I'm using the USB camera. But their is no preview & also not able to capture the images. In the kernel I have enabled the v4l2 drivers & the related tings by following/referring the TI sites. the web cam ( logitec c160 ) is detected & a device node video0 is created under /dev. from application layer the camera application is crashing. Also by analyzing the log according to my understanding i am thinking that it is referring to the ON board camera interface(CSI) & other errors like cameraservice failed, no device properties file found etc . from application layer to camera hal layers errors are there I think so. Please help me, what changes do I need to do to make the usb camera work & capture the images. Please help as I am in need of this for my project.
Here is my log 6523.logcat2_June21.txt
Regards
Sainath