Other Parts Discussed in Thread: OMAPL138, SMOMAPL138B-HIREL
Dear Sir/Madam,
I will like to find out the process technologies and ESD rating for the following part: SMOMAPL138BGWTA3R
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAPL138, SMOMAPL138B-HIREL
Dear Sir/Madam,
I will like to find out the process technologies and ESD rating for the following part: SMOMAPL138BGWTA3R
Thanks
Hello Nick,
I will check with our silicon experts and get back to you soon.
Regards,
Senthil
Hello Nick,
Please refer below the ESD ratings for OMAPL138 device.
You may refer to the OMAPL138 errata section 2.1.4 for the workaround to increase the system level ESD immunity.
http://www.ti.com/lit/er/sprz301m/sprz301m.pdf
You may also refer to the below e2e link where system level ESD immunity has been discussed.
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/238607/1123610.aspx#1123610
Regarding the process technology, Could you please elaborate your requirement ?
Regards,
Senthil
Hi Nick
OMAPL138 family is in 65 nm.
Since you are using Hi Rel variant , if you have queries specifically on the hirel part, I recommend posting queries on the HiRel E2E forum
http://e2e.ti.com/support/applications/hirel/default.aspx
Please make sure that you are looking at the hirel datasheet
http://www.ti.com/product/smomapl138b-hirel
and not the OMAPL138 commerical/industrial temp datasheet.
Regards
Mukul
Regards
Mukul