Other Parts Discussed in Thread: AM1808, OMAP-L138, DA8XX, PMP, OMAPL138
Hello
I've OMAP L138 LCDK kit i have audio file in file system i need to play the audio so tried aplay but its not playing the audio i got the following error
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AM1808, OMAP-L138, DA8XX, PMP, OMAPL138
Hello
I've OMAP L138 LCDK kit i have audio file in file system i need to play the audio so tried aplay but its not playing the audio i got the following error
Hi Sangly,
root@omapl138-lcdk:/aud# aplay -r 8000 t1.wavPlaying WAVE 't1.wav' : Unsigned 8 bit, Rate 8000 Hz, Monoasoc: machine hw_params failedaplay: set_params:1129: Unable to install hw params:ACCESS: RW_INTERLEAVEDFORMAT: U8
No its TI board not custom board.
i tried to play a audio via codec and headphone jack.
Hi,
What Linux SDK version are you using ?
MCSDK or Linux LCDK's SDK ?
Could you please share your bootup logs.
I'm using Linux LCDK's SDK
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
reading boot.scr
** Unable to read "boot.scr" from mmc 0:1 **
reading uImage
2040348 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.1.10
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2040284 Bytes = 1.9 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 3.1.10 (root@VPC-U1104) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #7 PREEMPT Fri May 11 11:15:57 CDT 202
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 LCDK
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyS2,115200n8 root=/dev/mmcblk0p2 rw rootwait ip=off
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 125856k/125856k available, 5216k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xff000000 - 0xffe00000 ( 14 MB)
vmalloc : 0xc8800000 - 0xfea00000 ( 866 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc0396218 (3641 kB)
.init : 0xc0397000 - 0xc03ba000 ( 140 kB)
.data : 0xc03ba000 - 0xc03db160 ( 133 kB)
.bss : 0xc03db184 - 0xc03f4c1c ( 103 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 148.88 BogoMIPS (lpj=744448)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 144 gpio irqs
NET: Registered protocol family 16
EMAC: MII PHY configured
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
Switched to NOHz mode on CPU #0
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
msgmni has been set to 245
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a 16550A
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a 16550A
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a 16550A
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver unknown
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
usb usb1: New USB device found, idVendor=1d6b, idProduct=0001
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: DA8xx OHCI
usb usb1: Manufacturer: Linux 3.1.10 ohci_hcd
usb usb1: SerialNumber: ohci.0
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM
TCP cubic registered
NET: Registered protocol family 17
davinci_emac davinci_emac.1: using random MAC addr: 46:44:c4:3a:46:ae
mmc0: new SD card at address 1234
mmcblk0: mmc0:1234 SA02G 1.83 GiB
console [netcon0] enabled
netconsole: network logging started
omap_rtc omap_rtc: setting system clock to 2012-04-11 04:56:43 UTC (1334120203)
mmcblk0: p1 p2
ata1: SATA link down (SStatus 0 SControl 300)
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
Freeing init memory: 140K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udevd (944): /proc/944/oom_adj is deprecated, please use /proc/944/oom_score_adj instead.
udev: starting version 141
Remounting root file system...
Caching udev devnodes
Populating dev cachemv: cannot rename '/tmp/devices': No such file or directory
NET: Registered protocol family 10
ALSA: Restoring mixer settings...
Configuring network interfaces... ifup: misplaced option " pre-up"
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Hardware abstraction layer hald
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: lighttpd.
2012-04-11 04:57:18: (log.c.166) server started
/
Starting Matrix GUI applicationdavinci_mdio davinci_mdio.0: resetting idled controller
net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:07, id=7c0f1)
ADDRCONF(NETDEV_UP): eth0: link is not ready
insmod: can't read '/lab1/armuga/driver/csscanner_fx2.ko': No such file or directory
insmod: can't read '/lab1/armuga/driver/csscanner_main.ko': No such file or directory
Setting IP sh/etc/rc5.d/S97matrix-gui-2.0: line 90: ./etc/init.d/configip: not found
.
PHY: 0:07 - Link is Up - 100/Full
ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org omapl138-lcdk ttyS2
Arago 2011.09 omapl138-lcdk ttyS2
omapl138-lcdk login:
Hi Sangly,
I'm also facing the same problem on Linux LCDK's SDK (kernel image) and I'm not getting any issues in MCSDK release SDK.
I will try to figure out that where is the problem.
Mean while please check in MCSDK.
Hi,
The below link is have latest MCSDK release for OMAPL138 (LCDK,SDI &EVM) with linux kernel ver3.3.
http://software-dl.ti.com/sdoemb/sdoemb_public_sw/mcsdk/latest1/index_FDS.html
Hi,
Got the sources.
copied the u-boot into SD card from mcsdk_1_01_00_02/images/u-boot-omapl138-lcdk.bin
by following command
desktop:/mediaAM1808/preparation$ sudo ./uflash -d /dev/sdb -b u-boot-omapl138-lcdk.bin -p OMAPL138 -vv
OMAPL138
U-Boot Size 356635
First partition starts at 32130(16450560)
U-Boot Magic Number : a1aced66
U-Boot Entry Point : c1080000
U-Boot Number of Blocks : 000002b9
U-Boot Starting Block : 00000075
Load U-Boot Address : c1080000
Writing U-Boot Signature
Writing U-Boot
Done...
copied the uImage into SD card (/media/boot)from mcsdk_1_01_00_02/images/uImage-omapl138-lcdk.bin and copied the filesystem into /media/rootfs
But its not getting boot i'm not getting any log.
Whats wrong in this what is the procedure to boot the board?
Hi,
You don't want to change the u-boot but just change the kernel (3.3) alone.
I tried but not booting successfully.
Its restarting
U-Boot 2010.12 (Aug 29 2012 - 10:07:08)
I2C: ready
DRAM: 128 MiB
NAND: NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
MMC: davinci: 0
U-Boot 2010.12 (Aug 29 2012 - 10:07:08)
I2C: ready
DRAM: 128 MiB
NAND: NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
MMC: davinci: 0
U-Boot 2010.12 (Aug 29 2012 - 10:07:08)
I2C: ready
DRAM: 128 MiB
NAND: NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit)
NAND bus width 16 instead 8 bit
No NAND device found!!!
0 MiB
MMC: davinci: 0
I followed the link http://processors.wiki.ti.com/index.php/OMAP-L138_Preparing_SD_Card_for_Boot
Please let me know what are images to be in SD card from mcsdk_1_01_00_02 and tell me the procedure ?
Hi,
You can follow the same procedure which you have done LCDK's SDK.
Procedure is the same for MCSDK and LCDK's SDK.
Ya i'm following same procedure but i cant't getting uboot log.
Which u-boot image i need to flash in SD card from mcsdk_1_01_00_02 ?
Hi,
Ya i'm following same procedure but i cant't getting uboot log.
Which u-boot image i need to flash in SD card from mcsdk_1_01_00_02 ?
We don't have separate procedure for MCSDK & LCDK's SDK releases.
How did you perform to boot the board with old u-boot or LCDK's SDK ?
You can use everything as it is from LCDK's SDK except kernel.
You may have bootable SD card for LCDK's SDK and replace kernel image only.
I flashed the LCDK image into SD card long back(6 months).
Now i formatted the SD card for new kernel, i forgot the procedure to flash the SD card so followed that link.
I took the mcsdk/images/uboot and signed by AIS tool then used the uflash tool to flash the uboot image into sd card but its not booting.
Can you share the AIS signed and working uboot and uImage (Linux 3.3) for LCDK to flash the SD card ?
And please tell the procedure to to flash those image into SD card.
Thanks
Hi Sangly,
For this SD creation, I have posted multiple replies in e2e forums, you can search in our forums and try to boot as like initial.
After that try to change the kernel (3.3) alone.